Part Number: CC3351 Hello,
I use the CC3351 RTOS SDK version R9.
When I use the wifi toolbox to decode logs from the CC3351 with the logger.bin from the SDK I can't have the logs in wirershark. I am using Linux/ubuntu. In fact I have the following…
Part Number: CC3351 Hello
May i kindly ask for your support for an issue we encoutered when testing Bluetooth
Bluetooth stops transmit after 200s after start testing
Also we observed that for longer measurements the Bluetooth need to be re-started…
Part Number: CC3351 Hello,
We are using the MCU R9 SDK with Zephyr RTOS. CC3351 is connected using SPI to a STM32 for WLAN and UART for HCI BLE.
We had a product which was working fine, the device was able to init CC3351 chip, doing BLE and wifi.…
Part Number: CC3351 Other Parts Discussed in Thread: CC33XX-SOFTWARE
Hello Do host MCU is able to switch CC3351 into the promiscuous/monitor mode? I would like to sniff 802.11 Management Frames in the surrounding and transfer them to host MCU over SPI…
Part Number: CC3351 Context: We're bringing up a CC3351 over SDIO (SDMMC2) using the CC33xx RTOS MCU Package, since the SDK doesn't ship a working SDIO driver/example (the bus_sdio.c platform glue exists but was a stub that ignored the isFixed parameter…
Part Number: CC3351 Other Parts Discussed in Thread: CC3300 , EZURI-3P-SONATI351 , Hi, We are trying to upgrade to the latest cc33xx 1.0.2.17 on CC3351. ti-linux-kernel: ti-linux-6.12.y (5ae038766eda6647bee6dc52c88308a0a280878d) cc33xx-linux-mpu-ports…
Part Number: CC3351 Hello TI ,
For OTP MAC address programming , TOKEN_ID is needed.
This ticket is for obtaining the TOKEN_ID
Thank you in advance.
Best regards, Lucian
Part Number: CC3351 Hello TI Team,
Hello TI Team,
We are evaluating the CC3351 for a project using the RK3568J platform running Android 12 (Kernel 4.19.232).
We noticed that TI has released patches for Linux Kernel 4.19 on your official GitHub repository…
Part Number: CC3351 Hi TI Team,
I am supporting a customer who is currently evaluating the CC3351 for a high-performance wireless audio application.
Instead of using a standard packaged IC or module, the customer is planning to take advantage of CC3351…
Part Number: CC3351 Other Parts Discussed in Thread: , CC3350MOD Hi all,
I am currently trying to integrate the BP-CC3351 board to our aarch64 platform via sdio. I am using Kernel 6.1.145. The module driver loads fine and i am also able to bring up…