Part Number: CC3351MOD Other Parts Discussed in Thread: CC3351 Hello All,
We are attempting to use Automatic Channel Selection (ACS) on CC3351MOD in order to better stream video in congested environments.
However, when setting channel=0 in hostapd…
Part Number: CC3351MOD The CC33xx Hardware Integration Guide (SWRU612A) states:
"RF traces must have 50Ohm impedance and must be no shorter than 9.24mm."
A minimum length requirement is unusual – typically RF trace guidelines define a maximum length…
Part Number: CC3351MOD Hello TI team,
On our product, the LOGGER pin for CC3351MOD is connected to AM6254ATLHJAMKR’s G21 / OSPI0_CSN1, which appears to have two modes: OSPI and GPIO.
Since the CC3351MOD logger pin requires 3M baud rate to properly…
Part Number: CC3351MOD Hi,
During FCC pre-compliance testing with CC3351MOD used in our design for BLE, we are observing an unexpected TX power drop for the 125 kbps, 500 kbps, and 1 Mbps PHY modes while using the default CC3351MOD cc33xx-conf-fcc.bin…
Part Number: CC3351MOD Other Parts Discussed in Thread: LP-XDS110ET , , CCSTUDIO We are using BP-CC3351MOD connected to LP-XDS110ET which is connected to a PC via USB-C. Additional power provided via Micro-USB-Connector.
Using Chrome on Windows. Installed…
Part Number: CC3351MOD Other Parts Discussed in Thread: CC3351 , Hello all.
Last year, I made a post regarding CC3351 WiFi module that would crash during video streaming.
Post: https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f…
Part Number: CC3351MOD Other Parts Discussed in Thread: CC3351 I am busy testing the TI CC3351 Wifi module on our custom PCB. It is currentlypaired with a MCU with Linux through SDIO interface.
I have noticed that in order to run pre-certification test…
Part Number: CC3351MOD Other Parts Discussed in Thread: CC3351 , Can the CC3351/CC3351MOD simultaneously operate BLE on 2.4 GHz AND Wi-Fi on 5 GHz at the same time? Are there any shared internal resources (PLL, synthesizer, baseband processor) that prevent…
Part Number: CC3351MOD Hi,
Our device should be able to use LTE and Wi-Fi concurrently. Apart from the certification concerns that implies, we would like to first make sure that coexistence can be managed properly on hardware side.
I saw in the CC3351MOD…
Part Number: CC3351MOD Tool/software: Hello,
Could tell us when this part will be in mass product and when can we we have sample for test it?
Best regards
Simon