Part Number: CC3501E Other Parts Discussed in Thread: CC3501 Tool/software: Hi admin,
When I import example of CC3501 SDK, CCS has eror: "This project was created for a device not currently recognized - Cortex M.CC35X1.".
CCS version: 20.0.1.4__1…
Part Number: CC3501E Tool/software: Hi Team
My customer is using CC3501ENJARSHR to build their own board.
And the board is now functioning normally. However, he observed an issue when both UART1 and UART0 are enabled simultaneously—the system crashes…
Part Number: CC3501E Other Parts Discussed in Thread: CC3501 Tool/software: Hi Expert,
can CC3501 do rssi calibration in production line?
Customer's target is to build a calibration table and get +/- 1dBm from -98 to 0dBm.
BR,
frank
Part Number: CC3501E Tool/software: Hi Team,
My customer is using CC3501ENJARSHR to enable wifi hotspot mode via 40 MHZ XTAL but it is not working.
The project: CC35xx_network_terminal is used and they perform the command : wlan_start and wlan_ap_role_up…
Part Number: CC3501E Other Parts Discussed in Thread: CC3501 , LP-XDS110ET , LP-XDS110 Tool/software: Hi Team,
My customer is using CC3501 to build PCBA w/ 40Mhz XTAL.
But they can not connect to WIFI Toolbox via LP-XDS110ET.
The following the…
Part Number: CC3501E Other Parts Discussed in Thread: CC3501 Tool/software: Hello Team, can I get the application schematics for CC3501, CC2755 (zigbee).
Part Number: CC3501E Other Parts Discussed in Thread: CC3561 , LP-XDS110ET Tool/software: Hi team,
I am working on a board which has CC3501E on it. Is there any requirements for the flash?
IS25WJ032F-JNLE is used for the dev board but I have put MX25R1635F…
Part Number: CC3501E Tool/software: 1. Does the Normal SPI can be used along with this MCU instead of Quad/Octal SPI?
2. Do the NAND Flash support for the MCU?