You can test the radio performance with the radio tool ( https://www.ti.com/tool/CC3XXXRADIOTEST ).
Since you are using the module it shouldn't be related to the Antenna (the device performs the required calibrations automatically - see chapter 4.9 in the…
Hi,
SmartRF Studio doesn't support these devices.
Do you mean Radio Tool?
There are 2 Radio tools. One works for CC3100 & CC3200 and the other one works for CC3xxx devices.
Please down load the Radio tool C3XXXRadioTest from the following…
Hi,
Radio tool version 1.2 is for CC3200 devices. For CC3220SF device you need to use CC3XXXRADIOTEST (current version v1.0.3.11).
(používáte špatnou verzi RadioTools, pro CC3220SF musíte použít CC3XXXRADIOTEST)
Jan …
Hi Derek,
You have wrong version of radio tools. For CC3120 device you need to use CC3XXXRADIOTEST not a CC3100-CC3200-RADIO-TEST . Latest version for CC3120 is a 1.0.3.11.
Jan
Hi Chris,
To answer your questions:
1. The recommended UART programmer is the XDS110. This is what comes with every CC32xx launchpad, as well as other TI connectivity devices such as the 13xx and 26xx.
2. The XDS110 is also a JTAG debugger, and is recommended…
Part Number: CC3120 Other Parts Discussed in Thread: CC3XXXRADIOTEST , , CC31XXEMUBOOST Hi team,
I’m working on Wi-Fi certification software for a product with the CC3120 Wi-Fi module on board. I’ve found the CC3XXXRADIOTEST tool, but noticed that it requires…
Hi Naveen,
I recommend referring to our certification page to download and review the CC3100MOD test reports along with other resources: http://www.ti.com/tool/SIMPLELINK-CC3XXX-CERTIFICATION
I also recommend utilizing the CC3100-CC3200 radio testing…
Hi,
How are you testing the CC3120? The CC31XXEMUBOOST does not have an MCU and only provides a COM port interface to your PC for programming, test and debug. What are you running on your PC to test the device?
I suggest you use radiotool to test out…
Hi Soumya,
You will want to use the Radio Tool for the CC3100 devices (CC3100-CC3200-RADIO-TEST):
www.ti.com/.../CC3XXXRADIOTEST
There is a guide for this tool here: processors.wiki.ti.com/.../CC3100_&_CC3200_Radio_Tool
Best Regards,
Ben M
Hi Wolfgang,
For such kind of usage is intended radio tools - www.ti.com/.../CC3XXXRADIOTEST
Here is description for Radio tools - www.ti.com/.../swru471 (see option Carrier Wave). Radio tools contains also host code, which can your customer integrated…