Other Parts Discussed in Thread: CC430F6147 , CC1101 I am programming two CC430F6147 MCUs with RF cores. The master sends a message to the slave, then slave is then supposed to send an acknowledgement and the master should light up an LED to show the receipt…
Other Parts Discussed in Thread: CC430F6147 I want to make my own prototype of EM4F6147RF900 module. Insteed of using SMA antenna i want to use Chip antenna in my module. can any one suggest which chip antenna i can use for CC430F6147 with the same balun…
Other Parts Discussed in Thread: CC430F5123 , CC430F5125 , CC430F5143 , CC430F5145 , CC430F5147 , CC430F6147 , CC430F5137 The IAR 5.40 release notes show added support for the following CC430's
CC430F5123
CC430F5125
CC430F5143
CC430F5145
CC430F51…
Hi Wouter,
I reproduced this behavior with CC430F6147 RevE on my bench. I also tried a CC430F6137 and this device worked fine under debug control.
I contacted our tools experts for detailed look into the debug stack. Can you please let me know which…
Other Parts Discussed in Thread: CC430F6147 Hi! I have CC430F6147 board. I'm setup MSCM1 = 0xEF, i hope state machine be in TX state, but they go to TX_UNDERFLOW. I transmit packet every 0,007sec. How i can stay in TX state whitout switch to IDLE or…
Leo, the packet sniffer doesn't detect the link to the CC430F6147. Is the tool compatible with the MSP-FET430UIF? See thread above.
How do I enumerate devices in Packet Sniffer?
Adding new applications and additional layers of software is NOT conducive…
Hey, you're racking up allot of Intellectual Points and I've got only 80 Prodigy!
It's looking like the MSP430 is the way to go, especially with the 8 ADC channels on the CC430F6147.
Important Question:
So, after starting up the Bluetopia…
Other Parts Discussed in Thread: CC430F6147 Hi all,
Just moved from IAR to CCS and now I am trying to find the number of cycles for a certain looping operation in my code running on CC430F6147. Without the cycle count enabled, everything is working fine…
Other Parts Discussed in Thread: CC2538 , CC430F6147 Hi,
Does anyone know, when the CC2538 will be available (samples, evalboard)?
(I see the reference design already online)
I'm in a process of designing a sensor node based on CC430 (CC430F6147), but…