Part Number: CC8520 Tool/software: Hi,
For programming during mass production, does TI provide a dedicated programming tool for CC8520? Is a debugger/programmer such as the CC Debugger provided by TI recommended?
Thanks,
Conor
Hi Toby,
When creating a control program for TLV320AIC3263 or TLV320AIC3262 and CC8520 using Purepath Wireless Configurator, the model numbers for TLV320AIC3263 and TLV320AIC3262 were not available in the Audio Interface Select device list.
I would like…
Part Number: CC8520 Tool/software: Hi,
The datasheet for the CC85xx series does not contain specific information on the input high voltage (VIH) and input low voltage (VIL) of various I/O pins such as GIO, I²C, and I²S. Is there any information on these…
Part Number: CC8520 Tool/software:
As shown in the figure, the SPI interface is used to program the chip.
Does this device have a way of reading Program memory data?
Part Number: CC8520 . We are designing a new replacement product and we may be able to keep using CC8520, but we need to add support for a new feature to send wireless MIDI over the “data side-channel.”
The maximum data rate would be a maximum…
Part Number: CC8520 Other Parts Discussed in Thread: CC2590 , CC2592 Hello,
Based on the "Application Note AN089 - Real World Range Testing Using CC85xx" , the application note states the range was increased to 130m+ when CC2590 range extenders…
Part Number: CC8520 Hi
I would like to know if CC85xx chipsets have security or encryption in the audio that is streamed from one device to the other.
Best Regards
Vijay
Part Number: CC8531 hello:
Our company has a number of wireless products that use cc8531. We hope to pair the host and slave through buttons.
I have some questions.
Do we still need to write the device ID in this way?
After the device is powered on…
Part Number: CC8520 Other Parts Discussed in Thread: CC2590 The wireless communication distance is about 8m, and the sound will be intermittent if someone stands in the middle. Hope to get your help, thank you. Is there a problem with software?