Part Number: CC8520 Hi,
Currently, CC8520 change the Tx power and frequency per GIO13 toggling for production line test and regulatory test.
is that possible to implement same function by I2C or SPI from MCU?
thanks.
Part Number: CC8520 Hi TI team,
I have a project use CC8520,When the fixed frequency modulation is 2.404Ghz and 2.460Ghz, the following waveform will appear,What is the reason for this?
Part Number: CC8520 Other Parts Discussed in Thread: CC2592 We have a design using the CC8520 together with a CC2592, and in general we are very satisfied with the results in performance and reach. However, we recognised a significant out-of-band peak…
Part Number: CC8520 hi,
1. Is there any driver demo for the Pure Path protocol Host-Controlled Operation mode? Where can I find the related demo?
2. Is there any driving routine of AIC3204 based on the mode of Question 1 above? Where can I find the reference…
Part Number: CC8520 Hi Sir,
I use CC8520 +AIC3204 for wireless micrphone.
In Autonomous Operation , it work well. When I use mcu to control the CC8520 for Host-Controlled Operation , it can be read the tow status bytes of cc8520 by mcu SPI interface.
…
Part Number: CC8520 Dears:
Use PurePath Wireless Commander to test the sensitivity of CC8520. Are there any guidance documents? Why can't we test the sensitivity of -87dBm in the CC8520 datasheet?
Part Number: CC8520 Hi team!
We are currently implementing our own PurePath module design. I was wondering if someone on the PurePath team knows if TI has done any studies on the relationship between signal strength, bit error rate and audio dropouts…
I would understand that the audio output of the receiver´s TAS5805 might be mute if the TAS5805 model is not correct and the volume control of the the TAS5805 does not work properly. But why would the CC8520 refuse to output the audio on the I2S interface…