Other Parts Discussed in Thread: CC8521 , CC2591 , CC2590 We have some questions about regulatory restriction by CC8521.
Q1) Can we pass each country’s regulatory by CC8521 + CC259x? Especially, we would like to know if CC8521 + CC259x can support TELEC…
I have a wrist-worn application (Lightglove) and need to transmit audio and non-audio data. Can my transmitter nest digital payload if my receiver knows when to listen to differentiate it? Also, can I access the USB port locally or only from the radio…
Other Parts Discussed in Thread: CC8521 Hi,
I used CC8521 to make a USB dongle,the hardware works good, but when I used the VOLUME bar(windows xp sp3) to turn down the volume, it didnt work. At last,I found that only the WAVE bar can be used to turn down…
Other Parts Discussed in Thread: CC8531 , CC8521 , CC8520 , CC2590 Hi,
Can I use the cc8521 /cc8531 to design the USB dongle as MASTER? Now I have got a CC8520 output SLAVE .
regards
Jack.
Other Parts Discussed in Thread: CC8521 Should a CC8521 USB dongle when connected to a USB port on a Windows PC cause Windows to search for a audio device driver? Where can I find the Windows drivers? The CC Configurator only comes with Cebal drivers which…
Other Parts Discussed in Thread: CC8521 , CC2590 Hi everybdy!
I'd like to know if the CC8521 (+CC2590) can be Tx and Rx contemporaneously and if it can be used also as a repeater for the audio wireless signal, possibly with two antennas.
Moreover…
Other Parts Discussed in Thread: CC8531 , CC8521 , CC8520 Hi,
Will the CC8521/CC8531 have the same pin-out as the CC8520? Just making sure that I can use the same footprint when these chips are released.
As usual thanks for all the help!
Yohan
Other Parts Discussed in Thread: CC8521
User guide for CC8521 states that USB functionality only works in “Autonomous Operation Mode”. In that mode, can the side channel data be still moved in/out of the external host? Can the USB interface protocol…
Part Number: CC8520 Other Parts Discussed in Thread: CC8521 , CC2590 , CC2591 Hello all,
Having exhausted my avenues, turning to you for advice.
I have had PCBs made from the Gerber files of the CC85XX-CC2590EM Reference Design.
Have built five of these…
Other Parts Discussed in Thread: CC8521 , CC8520 , CC8531 , CC8530 , CC2500 I need some verification on the PurePath wireless radio. I have some questions of the following parts:
1. what is the difference between CC8521 and CC8520?
2. What is th difference…