Part Number: CC8531 hi
Our company has a number of wireless products that use cc8531. We pair the host and slave through buttons.
We have some questions to ask you.
Question 1:
How can the CC8531 clear the slave pairing ID after successful pairing…
Part Number: CC8531 Our customer plans to use this solution to design a wireless microphone and need apply for certification of FCC ID, RED, SRRC, TELEC ID So below testing mode is needed: Hopping (low/middle/high channel), TX, all Data rate Non Hopping …
Part Number: CC8531 hello:
Our company has a number of wireless products that use cc8531. We hope to pair the host and slave through buttons.
I have some questions.
Do we still need to write the device ID in this way?
After the device is powered on…
Part Number: CC8531 Other Parts Discussed in Thread: TLV320AIC3204 , TLV320AIC34
Hi Team,
1. I use CC85XXDK-Headset on 1 master and 4 slaves. The 4 slaves perform audio input and send data to the host through wireless wave, and the host performs audio…
Part Number: CC8531 In "CC85XX_DK" EVM Board (CC85XXDK-HEADSET_UG.pdf) Press and hold the "CSN" port for power on/off to turn the power on/off. Can I change "CSN" port to Lock(High)= ON , unlock(Low)= Off?
Part Number: CC8531 Hello.
My product is undergoing a certification test.
The tester is asking for a hopping test mode, but I don't know what to do.
Because the
The tester is asking for a hopping test mode, but I don't know what to do. I modified…
Part Number: CC8531 Hi Team,
I currently need to use the device CC85DK-Headset to realize the uplink function in which one CC85XXDK-Headset should be connected to 2 Bluetooth devices. How should I configure it?
Kind regards,
Katherine
Part Number: CC8531 Other Parts Discussed in Thread: CC85XXDK-HEADSET-RD , CC85XX-CC2590EM-RD
Hi,
We are making a 4T -1R wireless microphone system,it works fine except that one out of 4 microphone will switch off automatically, and the time of duration…
Part Number: CC8531 Hello.
I have been developping a new product based on "CC85XX headset reference design 1_3".
Before developping, I have to test RF performance using PPWC (purepath wireless commnader).
How can I change the TX power of the…
Part Number: CC8531 Hi, TI support team
This is an inquiry about the inductor applied to the reference circuit below.
Does the value of 6N8 applied to L2, L5~8, and L10~15 have to be applied?
Why was the inductor applied to that part?
If it is deleted…