Part Number: CCSTUDIO Other Parts Discussed in Thread: AM2634 Hi,
In release note of CCS 12.6, I have seen that there is this new feature " Sitara MCU – JTAG flash programming support". I am currently working on a project with the Sitara AM2634 and…
Ki said: If the symbol or file is selected in the Modules view, in the context menu for it, select "Locate file" and browse to the appropriate file. This will configure the environment correctly and the debugger will open the correct files going forward…
Part Number: CCSTUDIO-SITARA Dear all,
we are working with AM263x Control Card Evaluation Module (EVM) to develop our project. During debug somentimes we need to reset and restart microcontroller but it doesn't work!!!
This problem also occurs with the…
Part Number: CCSTUDIO-SITARA Hi,
My customer is having some issue when connecting the AM3356(customer board) to CCS via XDS560v2 System Trace(Blackhawk). Their environment is : CCS v8.1.0.00011 is installed on Ubuntu 18.04. At target configuration, they…
Part Number: CCSTUDIO-SITARA We are using an AM2431 part on one of our products and I am trying to create a single image that contains the binaries that run on the M4, R5 and one of the PRU processors. I am using CCS12.0.0.00009 and themcu_plus_sdk_am243x_08_03_00_18…
Part Number: CCSTUDIO-SITARA Hi,
i have some java error by staring the debug server script. It happens at the Version 12.0.0. But not at 11.1.0.
~/ti/ccs1200/ccs/ccs_base/scripting/bin$ ./dss.sh ../examples/DebugServerExamples/msp430f5529_ccsSession.js…
Part Number: CCSTUDIO-SITARA Hi,
I'm attempting to create a new CCS project from scratch and I want it to have a sysconfig configuration. I was surprised to find there's no option to do that, at least not that I've found. The only way I've been able to…
Part Number: CCSTUDIO-SITARA Hi.
I used syscfg to add DDR to my existing project configuration. After rebuilding, I found that I was not completing the project generated initialization. It appears that I hit an error in Sciclient_init() at the last line…
Part Number: CCSTUDIO-SITARA I'm trying to enable DDR on the TMDS64GPEVM. I've enabled it on CCS using SysConfig. When I try to debug I get the following messages:
MAIN_Cortex_R5_0_0: GEL Output: CPU reset (soft reset) has been issued through GEL…
Part Number: CCSTUDIO-SITARA
Hi all
We use XDS110 to connected target and load program is OK,
when we use XDS200 to connected target ok but loading program is stuck on
How to solve this issue?
(1)XDS200 Test Connection pass
(2)XDS200 Loading program stuck…