Hi Greenja,
The Debugger DevPack was only designed with one purpose and that was to make an easy and cheap debugger of the SensorTag. The TM4C1294NC was never intended to be the host processor of the system.
Code composor studio will be free when used…
Other Parts Discussed in Thread: CCSTUDIO , SYSBIOS Hi,
I am trying to build the C674x DSP portion of MessageQ example on windows with CCSV5.1. The reason I am doing this is because I want to use CCSV5.1 debugger in my future development that resembles MessageQ…
Hi Sven,
Please ignore the patch in my previous post, and try this one instead. This patch has a potential fix for the performance problem.
Please let me know if it resolves the 3-5 minute delays you see.
Thanks,
- Baltasar
2526.com.ti.ccstudio.project…
David,
Here is the patch for issue #2.
To install the patch:
Make sure the user's CCS version is 5.3.0.00090 - the patch will only work on this build of CCS.
Download the attached file, and change its extension to ".jar".
Find the file…
Hi Erik,
The patch is attached. It is only applicable to CCS v5.2.1.00018, so please make sure that is the version of CCS that you have (see Help > About... dialog in CCS).
Please install the plugin into your CCS v5.2.1.00018 image as follows:
Close…
Part Number: CCSTUDIO Other Parts Discussed in Thread: ENERGYTRACE , , ENERGIA , CONTROLSUITE Tool/software: Code Composer Studio Attempting to install CCS V6.0.1.00040 fails to install after about 30-minutes of activity with a lengthy message indicating…
Part Number: CCSTUDIO Tool/software: Code Composer Studio Hi,
I'm attempting to install Code Composer on my Windows Subsystem For Linux, with no success. I'm running Windows 10 Pro, Build 19041.508 with Ubuntu 20.04 via WSL. I've downloaded the CCS 10…
Part Number: MSP430G2533 Other Parts Discussed in Thread: CCSTUDIO , ENERGYTRACE , ENERGIA , SEGGER , CC2538 , CC3200
Tool/software: Code Composer Studio
Log started 04/03/2017 at 17:26:28 Preferred installation mode : unattended Trying to init installer in…