Part Number: CD4051B-Q1 Other Parts Discussed in Thread: CD4051B , TMUX4051 Hello Sir:
We are using CD4051B-Q1 to design on our CVT controller.
Can you share the FMEDA document of CD4051B-Q1?
We need it to finish our FMEDA data.
Looking forward your feedback…
Part Number: CD4051B-Q1 Other Parts Discussed in Thread: CD40109B-Q1 Hi,
I'm interested in using the CD4051BQPWRQ1 and wondering what signal level the select lines should be at for VDD = 15V? Analog input signals would be in the 0 to +10V range.
Thank…
Part Number: CD4051B-Q1 Hello,
What will the switch state of CD4051B-Q1 be when power is not supplied and the INH pin is pulled down Low? Will the COM pin connect with any channel? Or, will all the channels be disabled?
The absolute Max rating of "DC…
Part Number: CD4051B-Q1 Other Parts Discussed in Thread: CD4051B , TS5A22364-Q1 , ADS1261-Q1 Hi colleagues,
I have some issues understanding the CD4051B-Q1 datasheet. In my system I have following supplies available: -2.5V, +2.5V and 3.3V. I need to pass…
Part Number: CD4051B-Q1 Hi Team,
My customer is designing the on board charger with CD4051B-Q1 and they want to use the SOIC package.
However, when checking the latest datasheet samples info. it seems for CD4051B-Q1 we only have the TSSOP package, but…
Part Number: CD4051B-Q1 Other Parts Discussed in Thread: DRV8847 , , SN74CBT3251 , MUX507
Hello, I'm trying to search for a 1:8 demux from TI.
I use MSP430G2 launchpad to generate PWM signals (10 ~ 10kHz, 1~60% duty cycle) and this is connected to…
Part Number: CD4051B-Q1 Other Parts Discussed in Thread: CD4051B Hi Team,
I want to know if CD4051B-Q1 can deal with rail to rail signal(0~5V signal) under following condition or not. I'm expecting that I can get we can get same voltage level signal from…
Xiao,
Figure 2 shows that there is a DC offset shift (not expected) of the input voltage up to 8 V compared to the Figure 1 offset 4V. Because the input voltage (11V) is greater than the supply voltage (8V), the output signal is clipped due to the…
Part Number: CD4051B-Q1 Hi All,
Are you planning any MSSOP / smaller packages (as AECQ100) for the CD4051/2-Q1 parts. Do you know if there is anything in the works or possible?
Thanks in advance!
Part Number: CD4051B-Q1 From email:
----
Hi Sonia,
I hope you are well. One of my customers asked if we are planning any MSSOP / smaller packages (as AECQ100) for the CD4051/2-Q1 parts. Do you know if there is anything in the works or possible?
Thanks…