Part Number: CD4504B I need voltage shifting from 3.3V to 12V in one application. Can I use CD4504B for the application? The connection of CD4504 will be like VSS-3V3, VDD-12V, SEL- 3V3. are those proper connections?
Part Number: CD4504B Hi team,
To rationalize the BOM I'm re-purposing the CD4504B to drive a BJT push-pull stage to feed a power MOSFET gate.
Since I only require 2 drives I have paralleled the inputs and outputs of the 4504 for increased sink &…
Part Number: CD4504B Hello, customer measured higher input current than max 1uA which is stated in the datasheet. Is this possible? He measured 4mA.
Regards, Holger
Part Number: CD4504B Other Parts Discussed in Thread: TLV1701 Hi All,
I have a 0 and 3.3V logic which should be conversted to 0 and 15Volt logic. Which IC you would recommend? There is an IC recommended in a thread is "TLV1701" but it has a delay of 500nsec…
Part Number: CD4504B Other Parts Discussed in Thread: CD40109B , TPL7407L , ULN2003B Hi Team,
Do we have new generation parts of high voltage level translation to recommend? Customer needs 8-channels, 3.3V in with 12V output, each channel should support…
Part Number: CD4504B Other Parts Discussed in Thread: CD40109B Hi Team,
I would like to find the level shift IC which could let voltage from 3.3V to 4V-10V or 4V-10V to 3.3V (Uni- directional)
I find cd4504b may meet my requirement, but i have not used…
Part Number: CD4504B Other Parts Discussed in Thread: TLV760 Hi team,
My customer is using CD4504B to convert a 3.3V input to 15V output. During the whole system is powered up, we found that VDD is powered up earlier than VCC. So there's a short period…
Part Number: CD4504B-EP Hi Team,
Do we have a SPICE MODEL for CD4504B-EP device? Can you share the model with me?
Looking forward to your inputs.
Regards,
-Renan