Part Number: CD74HC165 Other Parts Discussed in Thread: SN74LV8154 , PCM1794A
I built an entirely discrete logic based circuit and I have this shift register converting data from the Y bus on an SN74LV8154 to serial data and my logic design allows the…
Hi Ahmed and welcome to the forums!
TI doesn't directly provide libraries for every software platform out there, however we do provide detailed mechanical drawings in the datasheet (so you can make a footprint yourself) and the Ultra Librarian software…
Other Parts Discussed in Thread: CD74HC165 , CD74AC14 1)Dear Sir, please answer. I'd like to use CD74HC165 register with 3.3V supply and I need to connect Q7 output of the CD74HC165 to the input of CD74AC14 (3.3V supply too). I will not have problems…
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HCS165 , SN74LV165A , CD74HC165 , SN74HCS165-Q1 Is there p2p compatible one with new process as the Lead time of old one is not good? Pls recommend . Thanks
Part Number: SN74HC165 Other Parts Discussed in Thread: CD74HC165 , , SN74HCS165 , ISO7740 Dear,
the datasheet Note 2: When Vcc = 2V, Tt =1000nS =1000nS /V x (1.5V-0.5V) ? If Vcc=4.5V, Tt= 500nS/V x (3.15-1.35)=900ns, the chip will not be damaged. As…
I'm looking at how I could replace the microcontroller with purely logic components which synthesize a serial output just out of scientific curiosity but I'm having trouble with component selection, these components appear identical for instance: CD74HC165…
TI does not make any SPI I/O expanders.
To get pin-compatible crosses, you have to look for the name model number in another family.
For the SN74HC594: SN74AHC594, SN74LV594A. For the SN74LV165A: CD74HC165, SN74ALS165, SN74HC165, SN74LS165A.
I do…