Part Number: CD74HC4046A Other Parts Discussed in Thread: SN74HC4060 , Hi Team,
We would like to ask your help regarding the customer inquiry below.
Would like help defining / verifying / understanding resistor and capacitors (R1, C1, R3, C2 (R2…
Part Number: CD74HC4046A Other Parts Discussed in Thread: CD4046B , SN74LV4046A We need to use the CD74HC4046 in an already successful design of an instrument that uses an HCF4046, as the HCF4046 is now unobtanium. The PLL is used with a TI CD40103BE…
Part Number: CD74HC4046A Other Parts Discussed in Thread: SN74LV4046A Hi Team,
My customers are considering this device as a replacement of other products (Onsemi; MC74HC4046A).
However, the propagation delay is slower compared to other manufacturers…
It's possible - I don't see a specification for time to lock in the datasheet, so that might be a difference between the two that is undocumented.
Can they share a schematic? It's very difficult to troubleshoot a circuit that I have never seen.
Part Number: CD74HC4046A Hi Guys,
I have a 4V TTL signal operating at 200 kHz frequency(Input Signal can be seen in the figure attached) , i want to change its frequency to 400 Khz keeping the Voltage and waveform almost the same there can be a little…
Part Number: CD74HC4046A Hi Guys,
I have a 4V TTL signal operating at 200 kHz frequency(Input Signal can be seen in the figure attached) , i want to change its frequency to 400 Khz keeping the Voltage and waveform almost the same there can be a little…
Part Number: CD74HC4046A Hi all,
One customer use CD74HC4046 to make phase discrimination for two signals (1 hz). He wants to take advantage of the signal PC2out after filter as VCXO control signal. When PC2out disconnect to any devices, the phase discrimination…
Part Number: CD74HC4046A Other Parts Discussed in Thread: SN74LV4046A
Client is needing a custom FSK receiver that can demodulate 27.255 MHz carrier, where mark and space frequencies are only 4 KHz apart. I am reviewing Application Report SLAA618 that…
Part Number: CD74HC4046ACD74HC4046A can be implemented for fsk modulation and demodulation. Are there any other options in order to achieve PSK or QAM signal modulation in the same frequency range as CD74HC4046A.