Part Number: CD74HC4050 Does this IC provide Hysterisis?
The datasheet says turn On or VOH at around 3.15V for 5V VCC and VOL at 1.35V. So Technically there is hysteresis.
But when tested, both VOH and VOL are at VIH=VIL=2.2V. Can you clarify this?
Part Number: CD74HC4050 Hi expert,
Does TI provide double 85, 85% relative humidity and 85℃ temperature 1000 hours power-on test for CD74HC4050M?
BR
Emma
Part Number: CD74HC4050 Other Parts Discussed in Thread: SN74HCT244 , SN74AHCT125 , SN74AHCT367 , Hi expert,
If my customer use 5v power to CD74HC4050M96 VCC and use 3.3V MCU to drive the input.
so the input high will be 3.3V, and I suppose the 5v VCC will…
Part Number: CD74HC4050 Hi expert,
My customer hope to have the internal structure to better analysis the failure they meet.
I can see CD4050 have a internal structure:
and I each find the structure for HC type from toshiba:
https://toshiba.semicon-storage…
Part Number: CD74HC4050 Other Parts Discussed in Thread: SN74LV125A , SN74AHC125 I'm using a CD74HC4050D in a circuit where the input signal is 5v for HIGH , and 3.3V for HIGH on the output. I'm only using 4 of the buffers. Should the other two be: …
Part Number: CD74HC4050 Hello Guys,
Good day. Need your help in our customer concern on CD74HC4050E. Please see below in verbatim.
"I was using the CD74HC4050E buffer IC in between with a 100 Hz 5Vpk-to-pk 2.5V offset and 1% duty cycle input signal and…
Part Number: CD74HC4050 Other Parts Discussed in Thread: UCC28951 Hi
I have a customer who wants to power the CD74HC4050M96 device from 3.3V and drive the inputs from sources capable of 200mA (the sources are the OUTx signals from a UCC28951 SMPS controller…
Part Number: CD74HC4050 What is the IOH and IOL of the device?
How to calculate IOH and IOL values for the given load?
What is the max operating frequency of the device and how to calculate it?
Part Number: CD74HC4050 Other Parts Discussed in Thread: SN74LV367A Customer is using CD74HC4050 in a scenario where its VCC is turned off, but the logic on the load side of the buffer is not powered down (VCC = 5V). There is a pull-up resistor to VCC…