Part Number: CDCE72010 Other Parts Discussed in Thread: CDCM6208 , CDCE6214 Hello,
I am looking to upgrade my design from using the CDCE72010 to a fractional PLL (with one more more outputs) and was wondering if there are any components you may offer that…
Part Number: CDCE72010 I do not see where I can download version 1.3.1 (or later) of the CDCE72010 control GUI. This version has more controls than the available version 1.2.8.
Could you provide a download for this?
For reference, this is the thread…
Part Number: CDCE72010 Other Parts Discussed in Thread: LMK03328 , LMK05318B , LMK5B12212 Dear Team,
Could you recommend TI CLK-GEN? after base on my project clk frequency/ jitter request spec as table list, many tks!!
NO.
Frequency (MHz)
Clock…
Part Number: CDCE72010 Using the Evaluation board , CDCE72010EVM with the GUI interface to write to EEPROM. It appear to no changes on the write attempt. Change the U4, 25LC512 eeprom able to fix the problem?
Any way to check if the EEPROM is already locked…
Part Number: CDCE72010 Using the EVM board, program with EEPROM unlocked mode. To drive U1 PWR_EN driving low.
When change to external 5v supply, the value doesn't hold on. The U1 PWR_EN goes high.
Any recommended solution ?
Top op,
Step of programming and test usage:
connect usb to EVM board from a PC. JP_3_3 is selected at USB power supply
Open CDCE72010 Control GUI then load .ini file. (EVM board is working as intended with output of 491.52MHz)
Write EEPROM Locked with…
Part Number: CDCE72010 Hi Team,
Just double check for the Register 12 - bit 17:20 default value is 1111, it's RAM not EEPROM section, customer wants to double check if there is no way to we can fix this status value to 1000 after power up?
Or we must…
Part Number: CDCE72010 Other Parts Discussed in Thread: USB2ANY Hi Team,
I am helping customer trouble-shooting SPI command not working issue with USB2ANY.
I want to verify with expert if READ command is 0xCE (total 4 bytes) to read back status register…
Part Number: CDCE72010 I plan to drive PRI_REF with LVCMOS signal, meaning grounding the PRI_REF- with 1kOhm resistor as recommended in the datasheet.
However, I'm not sure what is the level of the signal that I should configure for PRI_REF+ while PRI_REF…
Part Number: CDCE72010 [TI-internal]
Hello team,
do we have any information about the longevity of CDCE72010?
The part had been released in 2008, so it is 13+ years in production already.
Thanks for any info on this.
Bartosz