Part Number: CDCE906 Other Parts Discussed in Thread: CDCI6214 , , CDCE925 I need to generate four independent clock frequencies that can be programmed by a microcontroller in the range of 500kHz to 1MHz. This is for a lock-in style design, so the output…
Part Number: CDCE906-706PROGEVM Other Parts Discussed in Thread: CDCE706 , My customer has not been able to get the CDCE706 USB EVM to work: https://e2e.ti.com/support/clock-and-timing/f/48/p/789126/2931472#2931472
They are now trying CDCE906-706PROGEVM…
Part Number: CDCE906-706PERFEVM Other Parts Discussed in Thread: USB2ANY Request:
The user guide of CDCE906PWR/CDCE706PWR refer: Connect the parallel port cable to PC and EVM parallel port.
But the demo lacks matching connect cable. According to the BOMs…
Part Number: CDCL6010 Other Parts Discussed in Thread: TMS320C6474 , CDCE906 , Hi All
I am using TMS320C6474 Mezzanine EVM Board by Spectrum Digital, without capability to read the on board eeprom (contain configuration registers for CDCL610 and CDCE906)…
Part Number: CDCE906 Other Parts Discussed in Thread: OMAP-L138 , Hi,
we are about to apply a CDCE906 clock synthesizer into our OMAP-L138 design. Hard- and software already works fine, in most parts.
The CDCE outputs the OMAP OSCIN clock of 24MHz, the…
I have the CECD906-706PERFEVM board, connected through a parallel port. The board wakes up with the default 27MHz output, but when I attempt to change the settings by selecting 'write register', I get 'write error' and no change in the output. …
Other Parts Discussed in Thread: CDCE906 Dear Sir
We have a project use CDCE906 to sync display clock
But this project we have 2pcs of CDCE906 can't workable
issue : Provide differential 100MHz clock input to CDCE906 and output provide 30Hz clcok…
Other Parts Discussed in Thread: CDCE906 Hi all Would you mind if we ask CDCE906? The datasheet on figure34 shows PLL Lock - Time from 81MHz to 297MHz. So, does it mean that PLL Lock - Time has proportionality? We need your help. Kind regards, Hirotaka Matsumo…
Other Parts Discussed in Thread: CDCE906-706PERFEVM , SN74LV125 Hi all!
We just bought two CDCE906-706PERFEVM boards, in order to simulate the system I am working on, but both of them seem not to output any signal. The user's manual states they should have…