Part Number: CDCE949 Other Parts Discussed in Thread: CLOCKPRO Hi Sir
May we must connect to EVM when we use TI Clock pro?
Because we have no EVM on hand.
may you pls help use TI Clock pro set CDCE949 Y2 output 66MHz,then output TXTfile to us for reference…
Part Number: CDCE949 Other Parts Discussed in Thread: LMK00334-Q1 , LMK00804B , hi dear supporting team,
for CDCE949-Q1,LMK00334-Q1,LMK00804B, if there are unused CLKIN, oscin, how to handle it? should we float it or AC couple to GND? and how about the unused…
Part Number: CDCE949 Hello,
I would like to create 25 MHz PLL out and I have found two PLL settings:
- Input clock is 27 MHz.
- Y7 is my target PLL in the attache TI Clock Pro capture file.
1. first settings (2015_1223)
M = 486
N = 3600
Pdiv…
Other Parts Discussed in Thread: CDCEL949 , CDCE949 , USB2ANY I am trying to programme a CDCE949 using the CDCEL949 evaluation board.
I have 4k7 pull-ups on my board and have disconnected R55 and R56 on the evaluation board and disabled the level translator…
Other Parts Discussed in Thread: CDCE949 For a number of years I've been using our stock of the now-discontinued Pletronics FD77T, which combined a pullable crystal and CDCE949 into a single package. Now that we're gearing up for production levels…
Other Parts Discussed in Thread: CDCE913 , CDCE949 Hi Team,
Is there any specific I2C programming sequence for CDCE913 and CDCE949 ?
Can you just start programming in order from Register 0x00h, 0x01h, 0x02h, ... , 0x1Fh ?
Please let us know if there is…
Part Number: CDCE925 Other Parts Discussed in Thread: CDCE949 Dears:
Do you have CDCE925 hardware reference design, the EVM reference design device is CDCE949, thanks!
Other Parts Discussed in Thread: CDCE913 Hi Team,
Please allow me to ask you about CDCE913,949 I2C programming. I believe you could program the device using block write.
[Question] Is there any limitation for byte size using block write command ?
Best Regards…