Part Number: CDCEL913 Other Parts Discussed in Thread: CLOCKPRO , CDCE913 , CDCE925 I would just like to confirm that the default Slave Address of the CDCEL913 is 1100101 b.
I know that address bits A1 and A0 are programmable, and the Configuration Register…
Part Number: CDCEL913 Other Parts Discussed in Thread: ADC3660 ,
I’m using a 12 MHz crystal oscillator and a CDCE(L)913 clock generator chip to drive the clock signals into an ADC3660. The CDCE(L)913 datasheet mentions an on-chip programmable load…
Hello Kia, I don't think to switch between LVCMOS and VCXO mode. I just want to use CDCEL913 under LVCMOS input mode. Then I just want to know whether we can use LVCMOS output type VCXO for clock source of CDSEL913 if we don't need to use CDCEL913's…
Part Number: CDCEL913-Q1 Other Parts Discussed in Thread: CDCE913-Q1 , CDCE6214-Q1 , CDCEL937-Q1 , CDCS503-Q1 Hi
The operational temperature range of CDCEL913-Q1 is only -40~85 while CDCE913-Q1 is -40~125, could you please tell me why? Any alternative part…
Part Number: CDCEL913 Hi Team,
Customer is consider use CDCEL913, but he wonders the phase noise about this product. Do we have that data?
By the way, what customer need is input 8MHz and output 64MHz, with lower power and low phase noise and jitter. 1…
Part Number: CDCEL913 Other Parts Discussed in Thread: CLOCKPRO Hi,
I am now trying to configuring the CDCEL913 to output the specified clock frequency on the Y1, Y2, and Y3 output.
By checking the data sheet, the chip will output 27MHz frequency on…
Part Number: CDCEL913 Other Parts Discussed in Thread: CDCEL9XXPROGEVM , Hi Sirs,
Sorry to bother you.
As title, we would like to know is possible to make CDCE (L) 913 burned in EEPROM when shipped.
Let 16.384MHz be Input, and 24MHz can be generated without…
Part Number: CDCEL913 Hi, Support team
My understanding is that the output on Y1 pin can be controlled by S0 pin. My customer think that they control Y1 output by GPIO of EC.
As shown at the following Table 6, Y1 is 3-state when S0=0 and Y1 is Enable when…
Part Number: CDCEL913 Hello,
We are currently evaluating the CDCEL913 for use in one of our designs and are interested in the spread spectrum clocking feature. We've got the CDCEL913PERF-EVM evaluation module and SSC is working just fine. However, section…
Part Number: CDCEL913 Hello,
I am using CDCEL913 to generate one 24MHz clock from output Y1,the input refclk is 25MHz crystal,PLL1 is used. And I use I2C to register the chip.
But the ouput is not right ,and the Fvco1_0 can not be set to more than 150MHz…