Part Number: CDCLVC1104 Hello,
Could you please recommend a military grade product that has the same or similar features as the CDCLVC1104PW?
Thank you.
Part Number: CDCLVC1104 Other Parts Discussed in Thread: CDCLVC1108 Hello:
Do you have Device Nomenclature about CDCLVC1104PWR? I haven't found in Datasheet.
like this below, Thanks!!!
Part Number: CDCLVC1104 Other Parts Discussed in Thread: CDCLVC1108 , CDCM6208 We are working at selecting an external clock source for the CLKIN inputs. The datasheet only specifies the slew rate for the inputs (1~4V/ns)
Can I get an answer on the following…
Hi Darren,
Sorry for the delay on updating this table. Please find below updates.
Parameter
CDCLVC1102/03/04
LMK1C1102/03/04
CDCV304PWR
Unit
Package
TSSOP (3.00 mm x 4.4 mm)
TSSOP (3.00 mm x 4.4 mm), WSON (2mm x 2mm)
TSSOP (3.00 mm x 4.4 mm) …
Part Number: CDCLVC1104
Hello,
According to the CDCLVC1104 datasheet, when VDD is 3.3V, the input voltage level conditions for the CLCLVC1104 are below.
When VDD is 3.3V, is it correct to input the clock to CLKIN only within the range of VIL and VIH…
Part Number: CDCLVC1104
Hi Team,
Good day! I am posting this in behalf of the customer.
I have shared the full details of inquiry below:
I’m using CDCLVC1104PW in order to buffer the incoming clock (100MHz-200MHz) from the FPGA (Spartan6) and apply them…
Part Number: CDCLVC1104 Other Parts Discussed in Thread: LMK1C1104 Hi team,
Is there any requirement for clock source in order to work with CDCLVC1104? Thanks a lot!
Br,
Nison
Part Number: CDCLVC1104 Hi,
There is some discussion on the device above with designers in my area. They believe there is a crystal or an oscillator in the device. I pointed out there is a ClkIn pin (pin 1) per the datasheet. So there is no internal…
Part Number: CDCLVC1104 Hi Team,
Can CDCLVC1104 direct replace CY2304NZZXI?
I see the output pin is not totally the same. Besides output pin, is there other spec difference we need to be aware of?
Thank you.