Part Number: CDCLVC1108
Sorry to bother, as the title, if customer want to use this device to fan out 120Hz clock, is it ok??
Anther questions, I saw "TI recommends placing the series resistor close to the driver to minimize signal reflection." from…
Other Parts Discussed in Thread: CDCLVC1108 Using the CDCLVC1108 to drive 8 output clocks to similar devices. F = 40 MHz. VDD = 3.3V, but receiving devices require clock signal between 1VPP and 2VPP. Trace length is about 100mm (50 ohm). Looking for a low…
Part Number: CDCLVC1104 Other Parts Discussed in Thread: CDCLVC1108 , CDCM6208 We are working at selecting an external clock source for the CLKIN inputs. The datasheet only specifies the slew rate for the inputs (1~4V/ns)
Can I get an answer on the following…
Part Number: CDCLVC1104 Other Parts Discussed in Thread: CDCLVC1108 Hello:
Do you have Device Nomenclature about CDCLVC1104PWR? I haven't found in Datasheet.
like this below, Thanks!!!
Other Parts Discussed in Thread: CDCLVC1108 , CDCV304 Hi,
Would you tell me about Operating Frequency for CDCLVC1108 ?
The datasheet says CDCLVC1108 operates from DC(0 MHz). Could CDCV1108 be used for 64kHz or less than it?
I've a similar question for CDCV304…
Other Parts Discussed in Thread: CDCLVC1108 There is a portion of CDCLVC1108 which is not known about calculation of powet dissipation. Please let me know the following.
------------------------ - Please teach me the calculation method of Pcload. ⇒Since…
Other Parts Discussed in Thread: LMK00105 , LMK00101 , CDCLVC1108 , CDCLVC1310 , CDCI6214 Hello.
Do we have solution to replace 9SBV0802 ? Thank you.
BR
Patrick
Other Parts Discussed in Thread: CDCLVC1108 , TXB0106 Hello,
I am using TXB0106PWR level translator in my circuit and i have a problem about translating to 5V from 3.3 V;
I use TXB0106PWR in my circuit as below:
I drive input port A (3.3 V) , but I can not…
Other Parts Discussed in Thread: CDCLVC1108 Hi My customer is using CDCLVC1108PWR. Could you let me know output current per pin which CDCLVC1108 can drive ? I think that it is 50mA per pin at Continuous output current of Absolute Maximum Ratings. Is…