Other Parts Discussed in Thread: CDCLVD110A We have an issue with correct programming sequence of the device via it's serial interface. The description in the data sheet is not very clear. Any example of working timing diagram of the serial interface…
Hi,
there is a pin named Vbb in CDCLVD110, and I don't know what it for. Is it for reference voltage used by external chips? If I want to use this chip driving FPGA's LVDS pins, can we ignore this Vbb?
THX!
Donald
Other Parts Discussed in Thread: CDCLVD110A I had query with respect to the LVDS specification.
We see that as per the datasheet the output voltage specified for 100 ohm load varies from 250mV to 600mV
Refering to the datasheet of CDCLVD110A we wanted…
Other Parts Discussed in Thread: CDCLVD110A Is it possible to drive CLK0/CLK1 inputs of CDCLVD110A with any other differential technology beside LVDS? If so, what would be the proper termination for driving an LVPECL signals to these differential clock…
Other Parts Discussed in Thread: CDCLVD110A The datasheet of CDCLVD110A only states a maximum input frequency.
Is there a minimum input frequency for this part?
thanks,
Adi
Part Number: CDCE72010 Other Parts Discussed in Thread: CDCLVD110A , Hello team,
I'd like to connect CDCLVD110A LVDS output to CDCE72010 PRI_REF pins with DC coupling.
Looking at the D/S, the CDCLVD110A VOS is 0.95 - 1.45V.
CDCE72010 Vicm is 1.0…
Part Number: CDCLVD1204 Other Parts Discussed in Thread: CDCLVD110A , , SN65LVDS2 Hello Experts,
There is a parameter of Vring, 10% max in CDCLVD1204 datasheet. Does Vring belong to any LVDS standard? I did not find this spec in CDCLVD110A datasheet…
Other Parts Discussed in Thread: CDCLVD110A , LMK01010 , CDCUN1208LP , SN65LVDS108 Hi Team,
The customer needs to select a clock buffer.
Here are the customer's requirements:
1. Input channel number: 1
2. Output channel numbers: 8~10.
3. Each…
A1. It should be OK
A2. If you need another PCIE buffer, we have CDCDB2000 which has 20 outputs and is DB2000QL compliant. You can also consider CDCLVD110A for a device with individual output enables. If you need a device with enables that disable a…
Hi Arvind-san,
Could I ask you a question again please?
I would like to propose TI clock driver instead of Cypress to my customer.
I looked into the device and I found CDCLVD110A. (1:10 Buffer)
Could you tell me more appipriate clock driver than…