Part Number: CDCLVP1102 Hi,
The differential output peak to peak voltage in the datasheet is 0.5V to 1.35V. Looks like it is a full frequency range spec in datasheet figure 2. my application is 80MHz, the typical value shall be close to 1.2V. What is…
Part Number: CDCLVP1102 Other Parts Discussed in Thread: CDCL1810 , CDCL1810A , Hi Sirs,
My customer is looking for a 1:2 fanout buffer device for CML levels, may I know there have any devices can meet this request?
Only one 100 Ohm termination for LVDS connection is needed, near receiver side (CDCLVP1102 input pins).
Figure 6 is DC coupling LVDS mode, Figure 7 is AC coupling Differential signal mode (including LVDS).
Figure 6 uses a parallel 100 Ohm. Figure 7…
Part Number: CDCLVP1102 Hi Team, Our customer would like to confirm if PECL/LVPECL is still recommended by TI for a new design as they find that there is a declining state on PECL/LVPECL from other suppliers. They are just looking for clarifications for…
Part Number: CDCLVP1102 Hi Team,
My customer would like to use CDCLVP1102 and the interface of receiver side is LVDS. we referred to app. note of SCAA059C for LVPECL to LVDS connection(Figure 5) and found two question. Please could team comment it.…
Part Number: CDCLVP1102 Other Parts Discussed in Thread: CDCLVP2102 , CDCLVP1204 , CDCVF2505 Hi team,
The customer is using CDCLVP1102. He uses the single-ended input. He tests the Vac_ref pin and it has a 2V voltage.
The schematic is in the attachment…
Part Number: CDCLVP1102 Other Parts Discussed in Thread: CDCLVD1204 , CDCLVD2102 , SN65LVDS105 Looking for a LVDS buffer –
requirement is 3.3V, 1:2 LVCMOS (single ended) to LVDS differential buffer, low jitter
Part Number: CDCLVP1102 Hello,
I would like you to confirm any clock buffer which relax input transition time.
According to datasheet of CDCLVP1102, min input edge rate is min 1.5V/ns.
Then, I would like you to confirm solution of one of below.…
Part Number: CDCLVP1102 Other Parts Discussed in Thread: LMK00334 Hi team,
customer is query if the CDCLVP1102 is suitable to use in the 1:2 PCIe clock buffer application? Please advise. Thanks.
Regards,
Arthur
Part Number: CDCLVP1102 I'm using 3.3v VCC. Section 6.8 of the cdclvp1102 data sheet list the Voh max as Vcc -.9 = 2.4V.
The Vol min is Vcc-1.7 = 1.6v. I would think the max Vout Diff p-p would be 2.4-1.6 = 0.8V.
The data sheet list the Max Vout Diff…