Other Parts Discussed in Thread: CDCM1802 Hi Sirs,
Sorry to bother you.
As title, Does CDCM1802 pin10/11 and pin2/3 need concern polarity??
Like Pin2 positive and Pin3 Negative?? Pin10 positive and Pin11 Negative??
Or doesn't matter?
Thanks for your…
Other Parts Discussed in Thread: LMX2571 , CDCM1802 I am working on a new design that requires a clock that can swing from 1-2MHz all the way up to 40-50 MHz, and possibly higher down the road. In the past we've used the LMX2571 for generating signals,…
Other Parts Discussed in Thread: CDCM1802 , LMK00306 Hello,
My customer have some questions about CDCM1802.
They want use CDCM1802 with LVDS input.
[Q1]
Input voltage swing between IN and _IN is listed as follows.
(A) VIN (Input voltage swing between…
Other Parts Discussed in Thread: CDCM1802 I am using the CDCM1802 to convert a single ended clock, to a differential LVPECL clock. I have it configured as a divide by 1. I have multiple circuit boards where the part is not operating as expected. The output…
Hi Nireeksha,
n times 100/3MHz, while n being a positive integer. Just mind the min max OSCin ranges.
Sure you can also use that buffer or LMK00105 or CDCM1802. LMK00105 has best performance for this task.
regards,
Julian
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: CDCM1802 , LMK00804B HI,
For the IC LMK00804B-Q1 , I am not able to find land patterns or dimensions in the datasheet. Can someone please help me with this.
I suggest CDCM1802 as a low-jitter buffer with programmable divide ratios (/1, /2, /4, /8) and supports differential or single-ended clock signaling on the input and output paths.
You may also refer to our part selector with clock buffer with dividers…
Hi Leo,
You may try cdcm6208V1 or cdcm1802.
6208 is a clock generator, it can take 44.1k to 192kHz signal in and then generate 2.8224MHz to 12.288MHz output.
1802 is a buffer with built-in div/4 divider.
Other Parts Discussed in Thread: LMK00105 , CDCM1802 , CDCE72010 , LMK01801 Currently we are using Clock buffer ( LMK00105) and Clock divider ( CDCM1802) separately on our board from TI. Now we are looking for Integrated chip where Clock Output 40MHz to be…