Part Number: CDCM61004 Tool/software: Hi team,
The manual describes that crystal is connected to the chip XIN at one end and the other end is grounded. Are there any detailed design references and precautions for this part of the circuit? I saw this…
Part Number: CDCM61004 Hi,
Could you tell me the recommended number of thermal vias? According to the recommended land pattern, there are only 5 vias, but Dissipation Ratings According to Note 2 of , there are 9 and the measurement condition is 4x4. Also…
Part Number: CDCM61004 Hi Team,
Do we have clock gen IC that can meet below requirements?
1. LVCMOS output frequency up to 1250MHz
2. Output Common Mode Voltage about 1.25V
3. Jitter below 50 fs rms
4. 3 ~ 4 ch LVCMOS output
Regards,
Roy
Part Number: CDCM6100XEVM Other Parts Discussed in Thread: CDCM61004 Tool/software: I am planning to order CDCM6100XEVM board. Could you let em know which clock generator is mounted on this board.
Is it mounted with CDCM61004? What is the part number…
Part Number: CDCM61004 We're using the CDCM61004 to provide (3) separate DDR4 input clocks to a Kintex Ultrascale device. We'd like to use the OSC_OUT line as the main clock input to the FPGA.
The datasheet references using OSC_OUT to "monitor…
Part Number: CDCM6100XEVM Other Parts Discussed in Thread: CDCM61004 Tool/software: I do not see a suggested layout in the CDCM61004 datasheet. Are the Gerbers available for the EVM board? Mostly concerned with the preferred placement of the REG1/2 caps…
Part Number: CDCM61004 Other Parts Discussed in Thread: CDCM6208 , CDCE6214-Q1 , LMK03328 Dear Sir/Madam,
We are planning to use the cdcm61004part in our design and design input details mentioned below.
Input type :CLKin, LVCMOS3.3V
Input freq:25MHz
Selected…
Other Parts Discussed in Thread: CDCM61004 Hello,
in the datasheet of the CDCM61004 the max. junction temperature is NOT specified. What is the max. allowed junction temperature ?
In my application the case temperature (top) is 90°C (worst case). The power…
Other Parts Discussed in Thread: CDCM61004 Hello,
in the datasheet Ican not find a specification of the frequency temperature drift. I supose that the temperature drift of the frequency is defined by the drift of the reference clock (crystal). Is my assumption…