Part Number: CDCM6208 We use only secondary input for xtal input and VDD_PRI_REF is left open, and PLL is not locked.
Do we have to connect VDD_PRE_REF to VDD if we don't use the primary clock input?
Part Number: CDCM6208 Hi, all!
I encountered a problem with this device:
In my board, PRI_REF pin is connected to a LVDS transmitter working at 100 MHz. SEC_REF pin(also VDD_SEC_REF) is directly connected to GND so it is not used.
REF_SEL pin is set to…
Part Number: CDCM6208 Other Parts Discussed in Thread: LMK5B33414 , LMK03328 , LMK5B33216 HI, Staff
I'm looking for a replacement for Clock Generator. Can you introduce compatible devices? Si5332E-D-GM2 → xxxxx Si53254A-D02AM → xxxxx Si5394E-A…
Part Number: CDCM6208 Hi,team
My customer has the following questions, can you help to answer them?
“We are checking the operation of the board equipped with CDCM6208V1RGZR. I was able to read the register by I2C, but I could not write it. The readout…
Part Number: CDCM6208 Other Parts Discussed in Thread: CDCLVC1104
Hi team,
Customer has some questions
When our company used TI chip CDCM6208, we found that the 40MHz spectrum characteristic of its configured output was extremely poor, which can be seen…
Part Number: CDCM6208 Hello,
Between part CDCM6208V1 & CDCM6208V1H there are differences in pre configuration setting. We had CDCM6208V1 on board, now this one is not available and i am getting CDCM6208V1H only, so I can directly replace the new one?
…
Part Number: CDCM6208 Hi,
One of my customers wants to know the difference between CDCM6208V1 R vs HR. It is not clear from the datasheet.
CDCM6208V1RGZR
CDCM6208V1 H RGZR
Thanks,
Soumya