Part Number: CDCS503 Other Parts Discussed in Thread: CDCE913
Tool/software:
Hello,
I want to use the CDCS503 as a clock multiplier in my circuit.
From the datasheet, the minimum clock input frequency is 8MHz.
I would like to drive a CMOS clock input…
Part Number: CDCS503 Tool/software: Hello,
I would like to use this clock multiplier in my circuit.
My supply voltage is V_DD=3.3V.
Fron the datasheet I know what its supply current when it works and outputs clock signal (OE input is high).
What is …
Part Number: CDCS503 Other Parts Discussed in Thread: CDCS504-Q1 Hello,
I'm comparing CDCS503 vs CDCS504Q1, specifically looking at cycle to cycle jitter. The 503 is spec'd at 110ps at 108MHz, and the 504 is 144ps at 11.264MHz. Because of the different…
Part Number: CDCS503 If using 2% Spread Spectrum reduces EMI, why would I select "no spread spectrum" as my option? Is there a tradeoff I need to know about?
Part Number: CDCS503 Hi team,
The datasheet states that the SSC_SEL0, SEL1, OE, and FS pins have internal pull-up resistors, but what are the resistor values? Also, can I connect an external pull-up or pull-down to each of these pins? If so, what is the…
Part Number: CDCS503-Q1 Other Parts Discussed in Thread: CDCE913-Q1 , CDCE6214-Q1 , CDCE913 , CDCE6214 , CDCEL913 Hi Sirs, Would you please provide a recommended part similar to CDCS503-Q1 but support 100MHz, 150MHz, 200MHz with +/-2% spread spectrum? Thank…
Part Number: CDCS503 Hi team,
My customer is considering to use the CDCS503. Could you support the questions below?
1. Is it okay if the SSCG input clock stops then returns?
2. Is it necessary to have a Delay time for the output to be valid after the input…
Part Number: CDCS503 Hello experts,
My customer is looking for the device which meets the requirement as below;
Input : LVCMOS 3.3V (4~12MHz)
Output : LVCMOS 3.3V, single channel
Multiplication : x2 ~ x4 (From 4~12MHz clock, they want to make max 25MHz…