Part Number: CDCV304 hi dear supporting team,
in customer's p/l, they found 3pcs CDCV304 CLKIN pin issue which pull the input signal voltage to 1V. below is the waveform they got in normal brd, pls help double check whether such overshoot will cause…
Part Number: CDCV304 Other Parts Discussed in Thread: LMK1C1104 We plan on using the CDCV304 as a clock buffer for our JTAG TCK signals. Does the CDCV304 require a continuous clock, or can the input clock start and stop (like what it does for the JTAG…
Part Number: CDCV304 Hi Team,
Good day.
My customer is looking to find the output impedance of the CDCV304 CMOS buffer over temperature. Or a min/max spec for the output impedance over the acceptable temperature range. Do we have this data?
The buffer…
Part Number: CDCV304 hi dear supporting team,
in CDCV304 D/S, there is only requirement on input voltage level, do we have requirement on input duty cycle and any other spec? tks a lot!
Part Number: CDCV304 Hi team,
Good day.
Our customer would like to know the HBM, CDM and MM ESD rating for the following devices:
CDCV304PWR
CDCV304PWRG4
CDCVF2310PWR
Thank you in advance for your help.
Regards, Carlo
Part Number: CDCV304 Other Parts Discussed in Thread: CDCVF2505 , Hi TI Expert,
In our design, CDCV304PW had be used for fan-out four 25MHz clock to CPU/CPLD/FPGA/PHY, we found 25MHz output duty cycle is 44.692%~45.150%, which not meet our applycation (45…
Part Number: CDCV304 HI team,
We find in generally CDCV304's unused pin is suggested to floating, but some customer designed the CDCV304's unused pin with a 4.7u cap to ground. Do you think there is any potential issue? thanks for your reply.
…
Markus Barthold said: In the design is for clocking the MCUs the clock buffer CDCV304 with an oscillator of 8 MHz. The clock buffer has no blocking capacitor and so there are spikes on the voltage supply.
Do you have the PLL enabled?
Can you cut the trace…