Part Number: CDCVF2505 Hi TI Team:
this device input/ouput has a positive clamp diode,When there's no clock input signal and VDD pin is 3.3V ,Whether CLKIN pin voltage is affected by VDD pin?
Part Number: CDCVF2505 Hi,
I understand that the feedback delay can be optimized by adding capacitor to CLKOUT pin, then can the delay of 1Yx pin be adjusted individually by adding capacitor to each 1Yx pins?
Best Regards,
Satoshi / Japan Disty
Part Number: CDCVF2505 Hi,
If we use 2 CDCVF2505s in series as follows,
Will the total jitter of the No.2 CDCVF2505 CLKOUT become OSC jitter + no.1 CDCVF2505 jitter + no.2 CDCVF2505 jitter?
and is there any point we should consider when we use them…
Part Number: CDCVF2505 Hi Team,
on the datasheet of CDCVF2505 first page you mention "Consumes Less Than 100 mA (Typical) in Power-Down Mode". The older datasheet revision mentions 100uA which sounds more likely. Can you please comment and adjust the…
Part Number: CDCVF2505 Other Parts Discussed in Thread: LMK04816 , CDCI6214 HI, staff
I'm looking for a feature equivalent device.
ispPAC-CLK5312S (Lattice) is looking for a substitute for EOS.
The requirements are ・ Input frequency: 44 MHz (※ It…
Part Number: CDCVF2505 Hi Team
I have a question with CDCVF2505. Adjustment capacity of delay time is shown in Fig.10 of p.11. Can I make a delay time of 2 nsec or more by increasing the capacity of CLKOUT? Is there a maximum delay time? Is it possible…
Part Number: CDCVF2505 Other Parts Discussed in Thread: LMK04208 , LMK04906 , LMK03200 , LMK01010 , LMK01020 , LMK01000 Hi Team,
Customer is looking for a solution creating propagation delay 2nS, the reason is if the reference clock to CPU and PCI IC…
Part Number: CDCVF2505 Hello E2E,
I have a customer asking about the max junction temp for the CDCVF2505PW. I didn't see anything in the datasheet. Do we have this data?
Thanks!
Russell
Other Parts Discussed in Thread: CDCVF2505 Hi,
Let me ask you following questions about CDCVF2505 please.
Q1) Input signal condition
When an input signal which has around 300ps jitter is inputted to CDCVF2505, the output jitter performace can be…