Part Number: CSD13381F4 Other Parts Discussed in Thread: CSD , CSD17382F4 , CSD13383F4 Hello,
I am using the CSD in the below circuit. the circuit opertes with either one of the FETs on or both off.
However when I have the upper FET disabled (0V applied…
Part Number: CSD13381F4 Other Parts Discussed in Thread: TINA-TI Hi Sir,
my we learn from you,
Refer to the following NMOS circuit diagram, input a square wave to the Drain terminal (point C1), and pull low from 3.3V==>0.1V, 3.3V==>0.2V, 3.3V==>0.3V,…
Part Number: CSD13381F4 Hi Sir,
could provide temperature curve for diode forward voltage? only 25 deg and 125 deg in SPEC.
we need -55 ~ 150 deg (include 0 deg), thanks for you help.
Part Number: CSD13381F4 Hi,
In CSD13381F4 12 V N-Channel FemtoFET MOSFET Top view a body diode is simulated between the source and the drain which is common and available in all the mosfets.
However, a diode between gate and source of the mosfet is also…
Part Number: CSD13381F4 Hi,
Can the CSD13381F4 Mosfet be switched ON using Vgs = 1.37 V?
In the schematic below, we will apply 1.37 V to switch LEDs on; can you please comment on the viability of our design?
Regards,
Faisal
Part Number: CSD13381F4 Hello,
I am using one of your mosfets CSD13381F4 to create a current sink in accordance with application note SLAA868. The circuit works perfectly, and I do get the current I need. However, I am using this same mosfet as well in…
Part Number: CSD13381F4 Other Parts Discussed in Thread: TIDA-00449 , CSD17318Q2 Hello,
i have a question about the mostfet used in TIDA-00449 for cell ballancing. So as this mosfet are very small and i can not solder it per hand can tell me which othe…
Part Number: CSD13381F4 Dear Expert,
Our customer are trying to find the distance and tolerance of the red part in below.
Could you help us to find it out? Thanks!
Regards,
Ben
Part Number: TIDA-00792 Other Parts Discussed in Thread: CSD13381F4 , , BQ76940EVM , TIDA-00255 Hi TI Engineer,
I am referring to TIDA-00792 hardware design files and found that CSD13381F4 FemtoFETs are (used for cell balancing) available only with LGA package…
Part Number: BQ2970 Other Parts Discussed in Thread: CSD13381F4 , BQ2980 , BQ2982 I'm looking at this part for protecting a rechargeable lithium coin cell, with maximum charge and discharge current about 50mA. Sizing the FETs for this is difficult; the math…