Other Parts Discussed in Thread: CSD16322Q5 , CSD16325Q5 Hi,
I need the FIT rates for CSD16322Q5 and CSD16325Q5 at 55C temperature with 60% confidence levels.
Can anyone provide this information. This is not available on the TI website.
Thanks…
Hi Tim, Thank you for your answer. I am sorry for this but it rose more question than it answers ! I will try with a csd16322q5, which seems to be equivalent to yours. The advantage is that we have it in stock so I should be able to give it a try today…
Part Number: CSD16325Q5 Other Parts Discussed in Thread: CSD16321Q5 , CSD17556Q5B , CSD16322Q5 , CSD16327Q3 , CSD17301Q5A , CSD17303Q5 , CSD17308Q3 Hi,
I am working on development of an application, which requires switching load through a mosfet. The…
Part Number: TPS51285B Other Parts Discussed in Thread: TPS51285A , , CSD17302Q5A
Tool/software:
Hi team,
customer want their switching deadtime could be larger than 10nS spec,
I know it's related to MOS Qg as well, but since it's fixed.
is…
Other Parts Discussed in Thread: CSD16325Q5 , CSD16322Q5 I need Cadence schematic symbols(*.sym) and pcb footprint(*.dra) for the following devices. If Cadence files are not available, then Orcad symbols and footprints will be acceptable. Can I get a…
Here's the config file I'm using. One more note: the current spikes that I see during the soft start happen at very regulatr 100 us intervals (10KHz).
UCD9224E @ PMBus Address 65d Project_Retries-On_170124B.xml
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…
Siyu,
I think the toggle flip-flop in the block diagram on page one of the spec should have let you know that the max you will get with this device is 50% duty.
Go to page 43 and 44 of the attached and select a more suitable part.