Part Number: CSD16408Q5 Hi,
I am using a gate Driver UCC27531DBV to drive the MOSFET CSD16408Q5.The simulation results were shown below w.r.t 3.3V and 0V Input Voltages to Gate Driver.
MOSFET having Vgs = 1.4V to 2.1V.
For the MOSFET to…
Jinting,
Please contact your local TI sales office or applications engineers you are working with. They will guide you through the process. If they are not familiar with your request, please refer to this post.
Thanks, JC
Part Number: TPS43060 Other Parts Discussed in Thread: CSD16408Q5 Hi,
I'm designing a product that need 24V / 1A output from 12V battery powered input. I choose the TPS43060 converter and we made some prototype boards. Most boards work as expected but…
Part Number: TPS7H4011-SP Other Parts Discussed in Thread: TPS7H4011EVM Hi TI support team,
We are working with Nokia for Space-grade project.
We are interesting in TPS7H4011EVM Evaluation Module, and need to implement to our project.
So We need…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…
Siyu,
I think the toggle flip-flop in the block diagram on page one of the spec should have let you know that the max you will get with this device is 50% duty.
Go to page 43 and 44 of the attached and select a more suitable part.
Peter,
i am enclosing the Power Management Guide for 2011. The section you will be interested in starts on page 43 and actual devices listed on page 46, With the minimum information you have given me I would expect that you will want something like…
Hi,
I've attached the 2013 User's Guide for power products. Starting on page 53 you will find a selection of PWM controllers. many of these teh frequency can be varied according to external criteria.
As an example if you use a UC3842 it is a simple…