Wen,
I am not sure I understand your question. The max Vgs of the CSD16570Q5B may be 20V, but the part can be operated all the way down to 4.5Vgs in the ohmic region, and even lower in the saturation region, where ORing applications typically occur.
…
Other Parts Discussed in Thread: CSD16570Q5B , TINA-TI Hi all Our customer needs TINA-TI model about CSD16570Q5B, so could you give us? The web offers P-Spice model for OrCAD, if you have general P-Spice model, could you give us? http://www.ti.com/jp/lit/zip…
Other Parts Discussed in Thread: CSD16570Q5B , CSD16556Q5B Hello Team,
My customer is interested in understanding if we can share and confirm from TI that the SOA limits for this part as shown in the datasheet is from measured data for the CSD16570Q5B? Can…
Part Number: UCC28780 Other Parts Discussed in Thread: , TIDA-010047 , CSD18510Q5B , CSD17570Q5B , CSD16570Q5B , UCC24612 , ATL431 , TL431 Hi,
Is it possible to achieve 92% efficiency using UCC28780 for Input line voltage 100VACrms to 130VACRMS and output 5V…
Part Number: CSD19501KCS Other Parts Discussed in Thread: CSD16570Q5B , I need the ESD spec, but we can't find on the datasheet and TI webpage.
Please let us know the ESD spec of csd19501KCS and CSD16570Q5B.
Part Number: CSD25402Q3A Other Parts Discussed in Thread: CSD25404Q3 , CSD16570Q5B , CSD17570Q5B Hi Team, I am designing a battery-operated system whose input charging current is about 10A maximum and the discharge current is up to 40A maximum. The 40A current…
Other Parts Discussed in Thread: CSD16570Q5B Hi team,
The application is 5V, 30A and the Vds voltage drop need to less than 20mV.
Do you have any recommend NMOS part?
Thank you!
Hello,
This is Akshay from Flex India.
We are currently working with one of our manufacturing plant to collect ESD(Electrostatic discharge) information.
The list for the required part no is attached.
Please help to provide the details ESD..xlsx .
Thanks…
Other Parts Discussed in Thread: CSD , CSD16570Q5B , CSD17570Q5B Hello,
We are interested in completing an NDA to obtain unencrypted PSpice (Level-3) models for NextGen FETs (CSD 16570 & CSD 17573).
Can you guide us on the process through TI AFA to accomplish…
The CSD95378B5QM is a Smart Power Stage. It takes a single PWM input, so you can't control the high and low fet individually. In an Hbridge setup you want to be able to PWM both the high and low fet individually.
All of our FET Power Modules are for…