Part Number: CSD17308Q3 Dear,
I use the CSD17308Q3 FET for a high-side switch as shown in the picture, in my circuit which imitates a TI's evaluation board of a driver IC, where the R1 = 5 KOhm, R2 = 10 Mega Ohm.
The application is Li-Ion battery…
Part Number: CSD17308Q3 Other Parts Discussed in Thread: CSD18543Q3A , CSD19538Q3A , CSD19537Q3 Hi,
I wanted to know the peak surge withstand voltage of CSD17308Q3
Is it 30V
thanks
regards
Subramani
Part Number: CSD17308Q3
I'm working on the next version of a wireless charger (board level design) at Earlens Corporation and have almost all of the critical components modeled with the exception of the CSD17308Q, to complete my analysis I need an unencrypted…
Part Number: CSD17308Q3 Other Parts Discussed in Thread: CSD25402Q3A , TINA-TI , CSD17578Q3A I am using the CSD17308Q3 in nine places of a design. The idea is to control the VGS of each of these CSD17308Q3 with independent isolated DC-DC converters (that…
Hello John,
I selected the CSD17308Q3 MOSFET for both and it works fine for PWM motor control but for boost converter I am still investigating on strange behavior on the boost converter overloading.
Best Regards,
Julien
Part Number: TPS40304 Other Parts Discussed in Thread: CSD16340Q3 , CSD17308Q3 , , CSD13202Q2 , CSD16301Q2 , TPSM82866A Hi,
I have designed the circuit from web bench power designer. Below is the attached snippet of my circuit.
Below is the reference snippet…
Part Number: BQ25723EVM Other Parts Discussed in Thread: BQ25713 , BQ25723 , CSD17308Q3 , CSD17578Q3A , , CSD18543Q3A Initially the power bank design was using the bq25713EVM circuitry . Since the bq25713 was unavailable, the bq25723 IC was dropped into the…
Other Parts Discussed in Thread: CSD17308Q3 My customer product is OCXO. It use TI CSD17308Q3; This OCXO need temperature on 110 degrees; product use Ampfier to driver MOS and MOS heat crystal through thermal conductive adhesive ; The early stage of the…
Part Number: BQ24800 Other Parts Discussed in Thread: CSD17308Q3 Hi
The application is conditioned as
VADP = 19V, VBAT = 16.8V, ICHG = 2A, FSW = 800kHz
During validation, we found the captured waveform with a bit of distortion on the low side drive…
Other Parts Discussed in Thread: CSD17308Q3 Hello
I use Orcad 16.5 Capture CIS and
I want to use Mosfet PSPICE model CSD17308Q3 for simulating dc converter.
but there is error and i don't know why.
here is error message.
"Subcircuit CSD17308Q3 used…