Part Number: CSD17506Q5A Other Parts Discussed in Thread: CSD13202Q2 Tool/software: Hi
Please let us know if this part can be used along with LTC4365IDDB#TRMPBF for 5V input. The recommended part in ltc datasheet is below but the part is obsolete. I…
Part Number: CSD17506Q5A Other Parts Discussed in Thread: CSD17577Q5A , Hi,
Customer is confused. Can you please specify which maximum current rating customer should take? 100 or 23A? And what is the difference? Thank you.
Best regards,
Ran…
Part Number: CSD17506Q5A Hello Team,
My customer has experienced a problem with the Ppspice model of CSD17506Q5A.
They entered an alternate node sequence 5 4 1. When they try to use the model with my symbols in ngspice it does not work
Compatibility…
Part Number: TPS40305 Other Parts Discussed in Thread: CSD17507Q5A , , TPS40304 , CSD17501Q5A , CSD17506Q5A Hi,
We have designed a circuit around the TPS40305DRCR.
Vin = 9V to 16V. Vin is connected to an external battery.
Vout = 5V/8A.
The MOS…
Part Number: TPS51120 Other Parts Discussed in Thread: CSD17527Q5A , , CSD17506Q5A Hi Sir,
We do glitch test for L/S gate by TPS51120 with CSD17527Q5A and CSD17506Q5A.
Below is capture waveform. May I know has any risk for MOSFET? Looks voltage is…
Hello Rick, I am working to find the reason for 2 days. I realized that the sound problem occured just after changing the limiting resistor. I needed to decrease the value of limiting resistor in order to get higher current values. Is there any specs…
Hi Yamaguchi-san,
Sorry for my misunderstanding. TI has many MOSFET package options including 2x2mm, 3x3mm & 5x6 SON and D2PAK. that can dissipate greater power than the Toshiba device. I did a search for FETs in these packages rated 30V to 60V and…
Other Parts Discussed in Thread: DRV8711 , DRV8711EVM , CSD18504Q5A Hello, I designed a stepper motor driver card with drv8711 and csd17506. Design schematic values same as drv8711evm user's guide.
My company using this card in our products and at least…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…