Other Parts Discussed in Thread: CSD17507Q5A , TINA-TI I only find spice model for power MOSFET CSD17507Q5A, which is not compatible with Tina.
I wonder where and how to get the Tina model for the power MOSFET and Transistors.
Thank you very much…
Part Number: TPS40305 Other Parts Discussed in Thread: CSD17507Q5A , , TPS40304 , CSD17501Q5A , CSD17506Q5A Hi,
We have designed a circuit around the TPS40305DRCR.
Vin = 9V to 16V. Vin is connected to an external battery.
Vout = 5V/8A.
The MOS…
Part Number: TPS53015 Other Parts Discussed in Thread: CSD17507Q5A , CSD86336Q3D , CSD86350Q5D , CSD87351Q5D Hi,
We are planning to use TPS53015 part in our board. Our system requirements are listed below.
1. 19V input (+/-5%), 3.3V Output Output…
Actually, the max VGS voltage of the CSD17327Q5A is too low. The CSD17507Q5A may be a better choice. The gate charge of that device is actually about 9 nC at 15 V, but that should still work for you. What is the equipment you are building?
Hi Kevin, As the file I atached above 5V-5A, I used WEBENCH tool on April2014. Now with the same input and output parameters, I can not select M1 and M2 with the same part CSD17507Q5A? Tks®ards,
Other Parts Discussed in Thread: CSD17507Q5A I'm trying to make the CSD17507Q5A (power transistor) part in a PCB Schematic/Layout. I saw on the TI webpage for this part the Ultra Librarian tool to create parts for layout, so I've downloaded that and the…
Thanks for feedback and sorry for delay. I was swithced to another project.
CSD175xxx series it's TI NexFET :)
CSD17507Q5A / 17510
i'll try to add it as my own part. thanks again
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…