Part Number: CSD17527Q5A Hi team,
My customer wants to use CSD17527Q5A to make a test board and they wonder if we can recommend some Driver IC.
BRs,
Peter
Part Number: CSD17527Q5A Other Parts Discussed in Thread: CSD17579Q5A Hi Sir,
Our customer want to know, If the CSD17527Q5A Working long hours on VDS=29.3V have any Risk?
Hugo
Part Number: CSD17527Q5A Hi,
It indicates the Max Pulse Drain Current is 85A in the datasheet, which is under condition that the pulse duration <=300us and the duty cycle <= 2%.
In application, If the current exceed 85A, but the duration is much…
Part Number: CSD17527Q5A Hi
How can I use the Pspice model of this component in pspice?
I'v got the error when running the program. The error is "Invalid device subcircuit".
thanks
Part Number: TPS23753A Other Parts Discussed in Thread: CSD17527Q5A Hello,
I want to use CSD17527Q5A NMOS in my boost converter. I am using PSpice software but unfortunately the pspice model of this NMOS is not working. I've got the error "Invalid device…
Two things. First, I intend to use this for 10-48V input and 12-48V output. The range I gave of 8 V and 20 V were just a few voltages that happened to work. So long term, 20/30V MOSFETs will of course not work. Second, I have managed to get this to "work…
Part Number: TPS23753A Other Parts Discussed in Thread: PMP9175 , CSD17527Q5A , CSD17551Q3A , CSD17579Q5A Hi
Our customer is considering PMP9175 for their design and the following question is coming out.
1. There are two FET like following figure and Q5 is…
Part Number: LM3152 Other Parts Discussed in Thread: CSD17527Q5A We are using an LM3152MH-3.3 part with two CSD17527Q5A FETs to generate 3.3V from a 24V input. We have recently had 2 of these circuits fail and have found that one or both of the FETs have…
Part Number: TPS51120 Other Parts Discussed in Thread: CSD17527Q5A , , CSD17506Q5A Hi Sir,
We do glitch test for L/S gate by TPS51120 with CSD17527Q5A and CSD17506Q5A.
Below is capture waveform. May I know has any risk for MOSFET? Looks voltage is threshold…
Hi Hao,
Now I using TPS65983 to act as USB PD Sources, Sinks, and Dual-Role Port application, I think TPS65983 can be able to do this.
I use the DC power supply to supply the PP5V0 and PP_EXT, and it is always powered. The external MOSFET is CSD17527Q5A…