Hi Steve,
I shared the schematic with you offline yesterday. Would you be able to take a look and see if anything jumps out?
On thing that stands out to me is that they decided to use the CSD88539ND instead of CSD17551Q3A (this is the one on the EVM…
Part Number: TPS23753A Other Parts Discussed in Thread: PMP9175 , CSD17527Q5A , CSD17551Q3A , CSD17579Q5A Hi
Our customer is considering PMP9175 for their design and the following question is coming out.
1. There are two FET like following figure and Q5 is…
Part Number: BQ25713 Other Parts Discussed in Thread: CSD17551Q3A , Hello.
I would appreciate some directions on how to use the formulae in the data sheet, section 10.2, especially section 10.2.2.5 (Power MOSFETs).
My design has the following requirements…
Li,
I choose the same NMOS whitch is used on the EVM , CSD17551Q3A. Both the Cg(Qg?)and the Rds_on are very low.
The highlighted lines are the switch node signal on my board(the resistances in series with the switching node signal are 0 ohm.), as shown…
Part Number: BQ25713 Other Parts Discussed in Thread: BQ24610 , CSD17551Q3A , CSD17578Q3A Hello,
I was wondering if the battery charge would be capable of charging an Ansmann 4S4P battery, The amount of cell the battery pack has is 16 Cells
Nominal Voltage…
Hi Yamaguchi-san,
Sorry for my misunderstanding. TI has many MOSFET package options including 2x2mm, 3x3mm & 5x6 SON and D2PAK. that can dissipate greater power than the Toshiba device. I did a search for FETs in these packages rated 30V to 60V and 10mOhm…