Part Number: CSD17570Q5B Other Parts Discussed in Thread: CSD17573Q5B Hello
What are the specific reasons/parameters why TI publishes " not intended for switching applications" for the low Rds N-FET 'CSD17570Q5B'?
Regards
Tom
Part Number: CSD16570Q5B Other Parts Discussed in Thread: CSD17570Q5B , CSD16556Q5B , CSD17573Q5B Hi team,
My customer need to find Pin to Pin device of both CSD16570Q5B and CSD17570Q5B, In fact, I have find some devices searched for similar products, but…
Part Number: CSD17570Q5B Hi Expert,
The application is from the redundant power supply.
The continue current will go through the body diode for a certain period.
Conditions:
Vo=12V
Io (into body diode) =31A
Duration=1.87mS
Pls advice how to know the…
Part Number: UCC28780 Other Parts Discussed in Thread: , TIDA-010047 , CSD18510Q5B , CSD17570Q5B , CSD16570Q5B , UCC24612 , ATL431 , TL431 Hi,
Is it possible to achieve 92% efficiency using UCC28780 for Input line voltage 100VACrms to 130VACRMS and output 5V…
Hi Shawn,
Thanks for reaching out to us. Please share the maximum capacitance value at the output of LM25069 and the timer duration. I would like to verify the MOSFET SOA margin. Generally, we recommend to use CSD16415Q5 due to better SOA as compared…
Part Number: BQ4050 Other Parts Discussed in Thread: CSD17570Q5B , BQ24600 Hi,
Configuration is as follows:
1. Using 4S1P lipo cells 8000mah
2. Load used while discharging of 7A
3. CSD17570Q5B (30V, 100A) as CHG and DSG FET
After charging the battery using…
Part Number: CSD25402Q3A Other Parts Discussed in Thread: CSD25404Q3 , CSD16570Q5B , CSD17570Q5B Hi Team, I am designing a battery-operated system whose input charging current is about 10A maximum and the discharge current is up to 40A maximum. The 40A current…
Part Number: TPS2412 Other Parts Discussed in Thread: CSD17570Q5B , TPS2413 Hi TI,
We have two VR for P5VA and P5VB and this design required redundant feature so we add two TPS2412 for oring control without active current sharing circuitry there due to…