Part Number: TPS2412 Other Parts Discussed in Thread: CSD17570Q5B , TPS2413 Hi TI,
We have two VR for P5VA and P5VB and this design required redundant feature so we add two TPS2412 for oring control without active current sharing circuitry there due…
Part Number: CSD18511KCS Other Parts Discussed in Thread: CSD17573Q5B , CSD17570Q5B , CSD18531Q5A , CSD18533Q5A , CSD18543Q3A , CSD88537ND , CSD18535KTT , CSD18540Q5B , CSD18536KCS , CSD18536KTT Tool/software: Hello Team, We are looking for some high…
Part Number: UCC28780 Other Parts Discussed in Thread: , TIDA-010047 , CSD18510Q5B , CSD17570Q5B , CSD16570Q5B , UCC24612 , ATL431 , TL431 Hi,
Is it possible to achieve 92% efficiency using UCC28780 for Input line voltage 100VACrms to 130VACRMS and…
Krishna,
Thanks for coming to us and asking about TI MOSFETs.
Unfortunately we do not have the same package as the SiE882DF.
The closest in silicon performance we could offer in a standard SON5x6 outline would be the CSD17573Q5B or potentially the…
Hi Rakesh
Thank you for reply.
Since it is a consideration stage on a desk, it is not possible to directly measure the temperature now.
Customers plan to use CSD17570Q5B × 2, but when the ambient temperature is 75 °C., do you need to determine…
Hi Shibin,
Thanks for your interest in TI FETs. Please refer to the blog in the link below. The maximum continuous current rating of 76A in the FET datasheet is a calculated value and assumes that the case of the device can be held at 25C. This implies…
Part Number: TPS2490 Other Parts Discussed in Thread: CSD17570Q5B Hello,
My customer is designing a hotswap circuits using TPS2490 and CSD17570Q5B.
Their requirements are as follows.
Vin=Vo=12V, Io=25.4A(max), Ta:0~+75oC
Cout=2460uF, ILIM=33A…
Hi Ricky,
Thanks a lot for the response. In my case I'd like to create own board, because features will be added.
So please what do you think about this configuration:
MCU: TMS320F28027F or 069M
NexFET MOSFET: CSD17570Q5B
Driver: DRV8305…
Wen,
Our best 25V device for ORing is the CSD16570Q5B. The best 30V for ORing is the CSD17570Q5B.
Both of these devices are significantly lower resistance than the Infineon device, and much higher Qg.
Why is the customer concerned about Qg? Is…