Part Number: CSD17579Q5A Other Parts Discussed in Thread: CSD17579Q3A Hello, I've been looking for the Pspice model of CSD17579Q5A, however, it seems that we have none both in its product page and spice rack.
I've noticed that CSD17579Q3A is somewhat…
Hi Visaacan,
To reduce the case temperature, you should be using thermal vias in the drain pad on the PCB that go to internal/back side copper shapes connected to the input voltage to the buck converter. You might also consider using a different low side…
Part Number: LM25149-Q1 Other Parts Discussed in Thread: CSD19502Q5B , CSD19505KTT , CSD18563Q5A , CSD18542KTT , CSD18534KCS , CSD17579Q5A , CSD17505Q5A , CSD16342Q5A , CSD15380F3 I've got a LM25149-Q1 design that simulates using the generic Pspice MOSFET models…
Part Number: CSD17577Q5A Other Parts Discussed in Thread: CSD17579Q5A Hi team
I have a customer who wants to use our MOS, and currently wants to use CSD17577Q5A or CSD17579Q5A, I would like to ask you if they have heat dissipation considerations, which…
Other Parts Discussed in Thread: CSD18514Q5A , CSD17579Q5A
This is a sinusoidal inverter.
Supply: 12V to 24V DC RMS, 100W
Input: I'll drive the PWM generator with a 100 kHz sinewave.
If the sine is 100 kHz, the PWM needs to be high enough to give a clean…
Dear Brigitte,
Thanks for the explanation
In the first batch (250 pieces) we used the CSD17579Q5A!
CSD17579Q5A {30 V N-Channel NexFET™ Power MOSFETs}.pdf
Do you have an idea why the measured ripple is so high... See below for the ripple
Best Regards…
Part Number: TPS40077 Other Parts Discussed in Thread: CSD17579Q3A , CSD17577Q5A , CSD17579Q5A , CSD17577Q3A Dear team
There is a good news that we design in TPS40077 in customer's new project.
The spec is Vin=19V,Vo=12V,Io=12.5A.
Could you help to review…
Part Number: LM3478 Other Parts Discussed in Thread: CSD17579Q3A , , CSD17579Q5A Tool/software: WEBENCH® Design Tools I changed two parts, because space requirements. These parts are:
D1 = SB20150TR to TSP20U60S S1G
and
M1 = CSD17579Q3A to CSD17579Q56
Can…
Part Number: CSD17527Q5A Other Parts Discussed in Thread: CSD17579Q5A Hi Sir,
Our customer want to know, If the CSD17527Q5A Working long hours on VDS=29.3V have any Risk?
Hugo
Part Number: LM3488 Other Parts Discussed in Thread: CSD19533Q5A , CSD17579Q5A , Hi, guys. I'm trying to make two custom PCBs with the LM3488MMX/NOPB. Each PCBs will have the MSP432P401R MCU (3.3V).
1) 5V micro-USB powered boost converter to generate…