Other Parts Discussed in Thread: CSD18501Q5A , CSD18502Q5B Dear sir
Why does Rthj-a always bigger then Rthj-c?
Is there a figure indicated specifically?
And I try use CSD18501Q5A in the load condition as follow
VDS:20V
Vgs: 7V
Peak Id: 100A/0.001s
Continue…
Other Parts Discussed in Thread: MSP430FR5969 , LM5017 , CSD18501Q5A I haven't had any luck exporting TI bxl files that use a power pad with less than 100% paste coverage to eagle PCB tools using Ultra Librarian. I am on the most recent release of both Eagle…
Benjamin,
PR2414 is a sync flyback converter with a 5V/2.3A output using the TPS23730. It shows the 24V input on the RJ-45 connector using the PPD pin, but the 24V can also be diode OR'd into VDD/RTN using the APD pin. I have attached the schematic…
Other Parts Discussed in Thread: TPS2491 , CSD18501Q5A Hello,
Is there a reference design for the TPS2491 using parallel FETs. I have nominal 24V power line that must be able to supply 33.3 Amps worst case. In addition to this I have a 30 mili-farad capacitive…