Part Number: CSD18504Q5A Tool/software: We have received parts with P/N: CSD18504Q5A, and we found there are excess residue since inside the reels/original from packaging. We unable to use this extra residue especially parts especially these parts are…
Part Number: CSD18504Q5A Other Parts Discussed in Thread: CSD18511Q5A Hello,
There is recommended stencil information in the datasheets of the below two devices.
CSD18504Q5A
CSD18511Q5A
But there is no information about its stencil thickness…
Part Number: CSD18504Q5A Other Parts Discussed in Thread: CSD18511Q5A Hello,
I have a question for the bellow devices.
・CSD18504Q5A
・CSD18511Q5A
Does TI recommend to use Pad-on-Via for Drain terminal of these devices?
Do you have any recommended…
Other Parts Discussed in Thread: CSD18504Q5A Hello.
My customer is currently in using CSD18504Q5A,now.
I have gotten a question about this product .
So, please teach me about CSD18504Q5A.
<Question>
Due to unforeseen circumstances,
does the…
Other Parts Discussed in Thread: LM3150 , TINA-TI , CSD18504Q5A , CSD18501Q5A , CSD18503Q5A I'm wondering the the CSD1850x family NexFET's are slated for TINA-TI model conversion any time soon. I noticed that quite a few of the lower voltage CSD FET's…
Part Number: CSD18501Q5A Other Parts Discussed in Thread: CSD18504Q5A , CSD18540Q5B , CSD19534Q5A Tool/software: We find following parts in our active BOM’s where in these parts are claiming the RoHS exemptions as mentioned below. We understand from EU…
Part Number: PMP10352 Other Parts Discussed in Thread: CSD18504Q5A Hi,
I am Guillermo Durà, from Magnetika.
We are trying to create our own transformers with litz wire and E cores. At this point, as a first prototype, we are using your PMP10352 isolated…
Part Number: LM3150 Other Parts Discussed in Thread: CSD18537NQ5A , CSD18504Q5A Hello Team,
I use this IC (LM3150MH_NOPB) for my DC DC converter, which has a 5V, 6A output and a 24 VDC input voltage. LM3150MH_NOPB
My output voltages are immediately…
Part Number: LM25149 Other Parts Discussed in Thread: CSD18514Q5A , CSD18504Q5A , LM5148 I'm making a design with LM25149
Design spec.: 15V to 28V input and 12V output, max current is 7.5A
I have used Webench for a design suggestion. Webench suggest…
Part Number: EM1402EVM Other Parts Discussed in Thread: CSD18504Q5A , BQ79616 Hello,
We are currently building modified EM1402EVM boards for our battery system. Many of the components used are unavailable or obsolete. Do you have qualified alternatives…