Please have a look at fet options in same package as EVM so it is easy to change. I will click TI thinks resolved and once you have the board and if you still have issues please contact.
Mathew
fet options.xlsx
Other Parts Discussed in Thread: CSD18509Q5B , CSD17303Q5 Hello to all,
Today I was looking for a setting in WeBench, want to enable automatic pic of same transistor for both, High and Low side transistors. Here is the sample schematics:
https://webench…
Thanks for the added information. I will give the CSD18509Q5B a try. We no longer have a TI Application Engineer in our area so I don't have any contacts to have a FW done.
Thanks,
Garrett
Other Parts Discussed in Thread: CSD18533Q5A , CSD18509Q5B Hello,
I'm working with BoosterPack + Launchpad in order to have a BLDC controller.
In the project, we need to support current of 35A to have maximum torque.
I am looking for alternatives to…
Hi Yamaguchi-san,
Sorry for my misunderstanding. TI has many MOSFET package options including 2x2mm, 3x3mm & 5x6 SON and D2PAK. that can dissipate greater power than the Toshiba device. I did a search for FETs in these packages rated 30V to 60V and 10mOhm…
Part Number: CSD18502Q5B Hi,
I have implement CSD18502Q5B power MOSFET which is driven by gate voltage via GPIO of MSP430. I need to supply 24V, 6A to a cooling assembly of an IR sensor.
I have attached the schematic with the post.
Please let me know…
Ian,
Sorry for the late reply. The Transient model nomenclature comes from the power products which may or may not need a transient and average (AC)model. The MOSFETs are transistor level based subcircuits and can be used in any simulation, hence the…