Part Number: LM25148-Q1 Other Parts Discussed in Thread: CSD18511Q5A , LM25149-Q1EVM-2100 , CSD18503Q5A , LM25148 , LM25149 , LM25149-Q1 Hi team,
As the title, could you kindly tell me what is the requirement of MOS? Do we have some recommended mos…
Part Number: CSD18504Q5A Other Parts Discussed in Thread: CSD18511Q5A Hello,
There is recommended stencil information in the datasheets of the below two devices.
CSD18504Q5A
CSD18511Q5A
But there is no information about its stencil thickness…
Part Number: CSD18504Q5A Other Parts Discussed in Thread: CSD18511Q5A Hello,
I have a question for the bellow devices.
・CSD18504Q5A
・CSD18511Q5A
Does TI recommend to use Pad-on-Via for Drain terminal of these devices?
Do you have any recommended…
Thank you for your answer!
We have questions about reference design TIDA-01557.
www.ti.com/.../TIDA-01557
(Question 1)
The output of this reference design is 1ch(12V).
But we want set two output(12V/7~7.5A and 24V/3.5~5.5A).
Standby power…
Part Number: CSD85302L Other Parts Discussed in Thread: CSD25402Q3A , CSD18511Q5A , CSD17575Q3 , CSD87313DMS , Hello,
I am trying to find the closest TI cross for a few FET parts. I have found what I think would be matches but I am looking for verification…
Part Number: LM5148 Other Parts Discussed in Thread: LM25145 , LM5143 , LM25148 Hello, We are designing a multibay charger and would like to use the LM5148 due to the CC control mode for charging batteries. We need applications help to understand how…
Nikolaus,
It is possible to use 30V FET with 24Vin. We see some customers do this, others prefer more headroom at like 40V. It really depends on what the ringing on the FET looks like.
You may have to use a snubber if you wish to use 30V devices.…
Please have a look at fet options in same package as EVM so it is easy to change. I will click TI thinks resolved and once you have the board and if you still have issues please contact.
Mathew
fet options.xlsx
Hi Yamaguchi-san,
Sorry for my misunderstanding. TI has many MOSFET package options including 2x2mm, 3x3mm & 5x6 SON and D2PAK. that can dissipate greater power than the Toshiba device. I did a search for FETs in these packages rated 30V to 60V and…
Hi Lutz, the industrial version needs to be republished as it has some errors, currently we are in that process.
Please use the following datasheet for now.
ucc25661.pdf
Regards,
Yamini.