Part Number: CSD18532KCS Tool/software: Hi team,
The drain pin and the case of CSD18532KCS and CSD15842KCS are not connected internally. Is my understanding correct?
Best regards,
Shunsuke Yamamoto
Part Number: CSD18532KCS Other Parts Discussed in Thread: CSD18543Q3A , , CSD18541F5 Hi Team,
A customer would like to amplify a 3.3V PWM signal into a 36V PWM signal.
Can you suggest the right device for the following requirements?
In: 300kHz…
Part Number: CSD18532KCS Hi,
I just dragged the current model of CSD18532KCS from the online TI lib to my schematic. And now I cannot simulate, because the model brings an error.
How can I fix it?
regards
Tiemo
Part Number: DRV8350R Other Parts Discussed in Thread: CSD18532KCS , DRV8350 , , CSD19532Q5B Can dvr8350R used to drive the CSD18532KCS 60V N channel MOSFET?
I have referenced the DRV8350 evm, It use the drv8350R to drive the csd19532q5b, I have found…
Part Number: CSD18532KCS Hi Sir, My customer use our CSD18532KCS for inverter 1000W project. Topology is push-pull with parallel FETs. High side 6 PCS / Low side 6 PCS. Currently have MOSFET damage issue, we find change gate resistor can improve this…
Part Number: CSD18532KCS Other Parts Discussed in Thread: CSD19536KCS , CSD19536KTT Hello team,
do we have any alternative to the is FDBL86062_F085?
I saw we do have some 100V devices but none of them seems to have a low Rdson.
Could you please…
Part Number: CSD18532KCS This Duke from WPI. I have FA case need you to help. Fail rate : 60/276 = 21.79% TI device : CSD18532KCS Use TI CSD18532KCS parallel 12 PCS application Inverter 2000W. (before use IR MOSFET solution) for burnning and life time…
Part Number: CSD18532KCS Dear all
I test the IDSS value, the test conditions are below:
VGS=0V,VDS=48V,environment temperature=25.6℃,humidity=56.88%RH
I had test 32pcs devices in total,among them 30pcs devices test the results are right, IDSS<1uA…
Carlos,
The CSD88599 will operate equally as well as the CSD18532KCS, it is possible to run the CSD88599 @ 100kHz, it simply comes down to powerloss at this higher than normal motor drive frequency.
Our apps team are on thanksgiving vacation, I will…
Part Number: CSD18532KCS Other Parts Discussed in Thread: CSD18510Q5B , CSD18532Q5B , CSD19531Q5A , CSD18533Q5A , CSD19502Q5B Hi Team,
My customer now facing delivery issue when using competitor's MOSFET. If TI have P2P P/N, customer will consider to…