Part Number: UCC27524A Tool/software: Dear TI Team,
Please find attached the reference circuit I am using. I am implementing the UCC27524AD as a driver in an interleaved PFC boost circuit (as per the attachment).
Currently, I am observing proper PWM…
Part Number: PMP11282 Other Parts Discussed in Thread: TL431 , UCC25600
Tool/software:
Dear TI Team,
I am working on the reference design PMP11282 Rev A , which is implemented on the PMP11064 Rev B PCB. I am currently facing an issue with the LLC…
Part Number: TPS43060 dear
TPS43060 input 18v outout 26v and ouput L=47uh,it will close output while output current is 5A, attachement is about Q2 waveform and SCH
and up and down drive is open in the meanwile, how to adjust het die area time of up…
LM5069.xlsx
I have uploaded the LM5069 Calculations. My Input supply ranges from 10V-30V. My OVL:30V and UVL:12V. Max Load Current: 8A I have chosen the Vishay SiJ186DP since there aren't any suitable TI mosfets in stock.
Part Number: UCD3138PSFBEVM-027 Hello, is the main circuit on the UCD3138PSFBEVM-027 development board using a diode-clamped advanced phase-shifted full bridge?
Some documents say that the loss of the lagging type is smaller, why do you choose the leading…
Hi,
wayne lu1 said:
Although I still need to use power line to transmit the data about the motor's speed or something else to control the motor.
So, do I need to buy a new device or any software I can use?
if you wish implement motor control…