Part Number: CSD18532Q5B ① Is Figure 12 in the data sheet the same when using both Ta and Tc? ②How should I consider Figure 10 in the data sheet using Ta (without heat sink)? ③Where is the current value that can flow through the diode between the source…
Part Number: CSD18532Q5B Other Parts Discussed in Thread: CSD19502Q5B Hi Team, seeking thermal information.
CSD18532Q5B
CSD19502Q5B
CSD96497Q5MCT
Thank you.
-Mark
Part Number: CSD18532Q5B Hello Guys,
Good day.
What is the Theta JC top (thermal resistance from junction to case top) for CSD18532Q5B ?
I found the forum post below, but seems to suggest that the RθJC on the datasheet is for the Junction to board.…
Part Number: UCC27511 Other Parts Discussed in Thread: CSD18532Q5B Hi team,
Customer is using our reference design PMP9656 to in their project. This design use 2 pcs UCC27511 drive 4 pcs MOSFET at the secondary side. And the MOSFET use CSD18532Q5B, it…
Part Number: DRV8701EVM Other Parts Discussed in Thread: DRV8701 , CSD18532Q5B Tool/software: Hi,
From the DRV8701EVM, the continuous current is 15A and peak current 20A.
Looking at the schematic of DRV8701EVM, the Vref is left floating, thus the current…
Part Number: CSD18532Q5B Hi Team,
Please help us with the below details for thermal analysis for CSD18532Q5B,
1. Max allowable case temperature
2. Junction to board thermal resistance
Part Number: CSD18532Q5B Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi,
I am trying to run a simulation in LTSpice using CSD18532Q5B, but the SPICE model appears to be encrypted. Where can I find an unencrypted version…
Part Number: LM5176 Other Parts Discussed in Thread: CSD18532Q5B Hi,
Would you please help review below 12V buck-boost VR?
PQ21 & PQ22 will be replaced with CSD18532Q5B (60V), please kindly review the design and get back to us, thank you.
SCHEMATIC1…
Part Number: DRV8701 Other Parts Discussed in Thread: CSD18532Q5B , Hello, I am using DRV8701E to drive a brushed motor. Unfortunately the driver goes into over current protection mode as soon as power is applied. The driver tries to reset ever 3ms for…
Part Number: LM5176 Other Parts Discussed in Thread: CSD17573Q5B , CSD18532Q5B
Tool/software:
Hello TI team,
have problems with my first LM5176 proto. I read now all other threads for LM5176, but will start with a bit generalized list of questions. Main…