Part Number: CSD18563Q5A Other Parts Discussed in Thread: CSD19533Q5A , CSD18533Q5A Hi,
Our End customer is asking if there is an Alternate Part/Equivalent for CSD18563Q5AT
Part Number: LM5143 Other Parts Discussed in Thread: CSD18533Q5A , CSD18563Q5A , LM5145
Hi, Just downloaded the Synch Buck calculator from ti.com, and for one of their synch buck chips, i got it to calculate the switching loss. It said top FET switching…
Part Number: LM5145 Other Parts Discussed in Thread: LM5146-Q1-EVM12V , CSD18563Q5A , CSD18533Q5A , LM25137 Tool/software: Hello!
I am designing a voltage regulator using the LM5145. The input range is 15-52V, and the output is 12V at 10-12A. I have…
Part Number: CSD18531Q5A Other Parts Discussed in Thread: CSD18533Q5A Hello,
Could you confirm whether the junction-to-case thermal resistance (1 W/C) given for this part (CSD18531Q5A) is to the case top or bottom?
Also, do you have a junction-to…
Part Number: LM5145 Hi
I have a problem with LM5145. My system requirement like that;
Vin = 27-40 V
Vout= 24 V
Iout = 10 A
I prepared my circuit according to WEBENCH POWER. I used CSD18533Q5A as mosfet.
But when ı power on to system, high…
Hello,
If you are not driving very much current into the motor, it could take some time for the low-side MOSFET body diode to move through reverse recovery.
You may want to try an experiment using CSD18533Q5A (P2P), since it has a much lower Qrr…
Part Number: CSD18534Q5A Other Parts Discussed in Thread: CSD18543Q3A , CSD18531Q5A , CSD18533Q5A , I CAN import the Pspice models into ADS for: CSD18531Q5A & CSD18543Q3A.
But you cannot import the Pspice models into ADS (2016 or 2019, doesn't matter…
Part Number: CSD17576Q5B Other Parts Discussed in Thread: CSD18533Q5A , CSD87333Q3D Hi all,
Can I know the ESD rating about CSD17576Q5B and CSD87333Q3D? My customer is asking the spec. about those devices (and CSD8530Q2/CSD18533Q5A but I've find post…
Hello Sv,
Thanks for the updated information. For 24V peak input voltage, you should be able to use a 30V FET. I'd recommend the CSD17573Q5B, 30V N-channel in 5x6mm SON package. The conduction loss for each FET at 40A is about 2.3W at TJ = 100°C and…
Part Number: DRV8353R Other Parts Discussed in Thread: DRV8301 , DRV8353 , MOTORWARE , CSD18533Q5A Hello,
I swapped DRV8301 with DRV8353 on a already working design but I obviously have issues with the gate drive control.
I run motorware lab 1c which…